Skip to main content
jacopokunak
Associate III
April 8, 2025
Solved

CubeMX MDF/ADF Driver for STM32U3 does not build

Hi,

I have a project working on a STM32U5 and I was curious to port it to STM32U3 to see the differences in power consumption.

I have built the project for the STM32U3 with CubeMX with the firmware packet "FW_U3 V1.1.0" , which is currently the latest available.

My project uses ADF1 to acquire the signal from a digital microphone among other things.

I configured all the pheripherals and added my code without any problem but when I built the project the mdf.c source file in function "void HAL_MDF_MspInit(MDF_HandleTypeDef* mdfHandle)" (which is automatically generated by CubeMX) gave me an undefined reference error for this definition "IS_ADF_INSTANCE(mdfHandle->Instance)".

IS_ADF_INSTANCE() is missing.

I look into my STM32U5 project and this Macro is defined in file "stm32u5xx_hal_mdf.h" .

I added it manually into the USER CODE of my STM32U3 mdf.c file and the project builds perfectly.

 

Please check the next release MDF/ADF drivers that are released for CubeMX, since this automatically generated code should be bug free. 

This topic has been closed for replies.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
July 9, 2025

Hello @jacopokunak;

 

The issue is fixed in STM32CubeMX 6.15.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.

2 replies

KDJEM.1
ST Technical Moderator
April 8, 2025

Hello @jacopokunak ,

 

Thank you for bringing this issue to our attention. 

I reported internally.

 

Internal ticket number: 207079 (This is an internal tracking number and is not accessible or usable by customers).

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
KDJEM.1Best answer
ST Technical Moderator
July 9, 2025

Hello @jacopokunak;

 

The issue is fixed in STM32CubeMX 6.15.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.