Skip to main content
imi415
Associate
June 7, 2018
Solved

CubeMX Makefile Generator Reported Error while Updating Project

Posted on June 07, 2018 at 18:44

After updating to CubeMX 4.26.0, Makefile projects cannot be updated due to the following errors:

0690X0000060BanQAE.png

2018-06-08 00:35:55,360 [INFO] ToolchainGenerator:120 - stack trace : java.lang.UnsupportedOperationException: Not supported yet.

at generators.MakefileGenerator.updateHeapAndStack(MakefileGenerator.java:315)

at generators.Generator.generateLinkerFile(Generator.java:715)

at generators.Generator.copyLinkerFile(Generator.java:407)

at convertor.Convertor.generateMakefile(Convertor.java:1436)

at convertor.Convertor.generate(Convertor.java:608)

at convertor.Convertor.convert(Convertor.java:515)

at convertor.Convertor.updateProject(Convertor.java:384)

at com.st.microxplorer.plugins.projectmanager.model.ToolchainGenerator.update(ToolchainGenerator.java:114)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createToolChainFolders(ProjectBuilder.java:1780)

at com.st.microxplorer.plugins.projectmanager.engine.ProjectBuilder.createProject(ProjectBuilder.java:574)

at com.st.microxplorer.plugins.projectmanager.engine.GenerateProjectThread.run(GenerateProjectThread.java:41)

#stm32cubemx.
This topic has been closed for replies.
Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
June 27, 2018
Posted on June 27, 2018 at 19:10

Hi All, 

There is an issue with regeneration of makefile project with the 4.26.0.

This will be fixed in the 4.26.1 which will be on the web soon

11 replies

Khouloud GARSI
ST Employee
June 8, 2018
Posted on June 08, 2018 at 09:45

Hi

Sun.Sim

‌,

This is reported to our CubeMX team. One of our experts will answer you ASAP.

Khouloud.

Gavriil Pascalau
Visitor II
June 8, 2018
Posted on June 08, 2018 at 15:47

Hello,

I have the exact same problem when generating the Makefile.

Khouloud GARSI
ST Employee
June 8, 2018
Posted on June 08, 2018 at 15:59

Hi

gavriil.pascalau

‌,

This is already under check.

Thanks for your comprehension and sorry for such inconvenience.

Khouloud.

chaoyu chen
Associate
June 15, 2018
Posted on June 15, 2018 at 10:36

I also encountered this problem! Please help to solve it. Was stuck here.

Nicolas Ducho0ud
Visitor II
June 18, 2018
Posted on June 18, 2018 at 12:01

Same problem since update to new cubemx 4.26.0

Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
June 27, 2018
Posted on June 27, 2018 at 19:10

Hi All, 

There is an issue with regeneration of makefile project with the 4.26.0.

This will be fixed in the 4.26.1 which will be on the web soon

yuqlid
Visitor II
July 24, 2018

Today, I tried the 4.26.1.

but, this problem wasn't solved...

VPand
Visitor II
August 13, 2018

Hello,

I'm facing this issue with KeilProject and TrueStudioProjects also. Version 4.26.1. Problem is still not solved.

imi415
imi415Author
Associate
August 13, 2018

However, after recent update to 4.26.1, project generator is completely unusable..

Code generation succeed while project generation always failing.

Updated system Java to 10 solved everything.

Makefile re-generation still fails.

Everything unstable now...

Beni1
Associate II
August 15, 2018

Hi,

Having the same issue with version 4.26.1 here too, when regenerating a Makefile project. Any updates?