Skip to main content
HMüll.4
Senior
May 20, 2022
Solved

CubeMX: how to get data when callback is called?

Hi,

I'm trying to read data from the SPDIF-input of the STM32F466 using the CubeMX-generated code. The idea is to get one interrupt/callback for every pair of audio samples which arrive. This looks good so far, there is a function HAL_SPDIFRX_RxCpltCallback() which has o be overwritten in own code section.

Now the question is: when this callback is called, how can I get the related data? Is there an other function to get these data or do I have to read some registers directly?

Or more generic: is there a manual available that describes these CubeMX-generated functions?

Thanks!

This topic has been closed for replies.
HMüll.4
HMüll.4Best answer
Senior
May 20, 2022

OK, found it in the structure that is handed over as parameter to the callback - please ignore this question!

1 reply

HMüll.4
HMüll.4AuthorBest answer
Senior
May 20, 2022

OK, found it in the structure that is handed over as parameter to the callback - please ignore this question!