Skip to main content
rb1
Associate II
Apr 16, 2020 8:39 AM UTC
Question

CubeMX generates wrong function call when remapping input capture TIM16/TIM17

When I enable TIM16 and TIM17 for a project on the STM32H753ZI in CubeMX (version 5.6.1) and I select Input Capture direct mode from Remap, I can select TI1 remap capabilities (see picture below).

0693W000000VulBQAS.png

The generated code below is not correct. Line 17 calls HAL_TIMEx_RemapConfig() which is not suitable for this timer. The code should call HAL_TIMEx_TISelection(&htim17, TIM_TIM17_TI1_RCC_HSE1MHZ, TIM_CHANNEL_1) instead.

/**
 * @brief TIM17 Initialization Function
 * @param None
 * @retval None
 */
static void MX_TIM17_Init(void)
{
 
 /* USER CODE BEGIN TIM17_Init 0 */
 
 /* USER CODE END TIM17_Init 0 */
 
 TIM_IC_InitTypeDef sConfigIC = {0};
 
 /* USER CODE BEGIN TIM17_Init 1 */
 
 /* USER CODE END TIM17_Init 1 */
 htim17.Instance = TIM17;
 htim17.Init.Prescaler = 0;
 htim17.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim17.Init.Period = 0xffff;
 htim17.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;
 htim17.Init.RepetitionCounter = 0;
 htim17.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_ENABLE;
 if (HAL_TIM_Base_Init(&htim17) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIM_IC_Init(&htim17) != HAL_OK)
 {
 Error_Handler();
 }
 sConfigIC.ICPolarity = TIM_INPUTCHANNELPOLARITY_RISING;
 sConfigIC.ICSelection = TIM_ICSELECTION_DIRECTTI;
 sConfigIC.ICPrescaler = TIM_ICPSC_DIV8;
 sConfigIC.ICFilter = 3;
 if (HAL_TIM_IC_ConfigChannel(&htim17, &sConfigIC, TIM_CHANNEL_1) != HAL_OK)
 {
 Error_Handler();
 }
 if (HAL_TIMEx_RemapConfig(&htim17, TIM_TIM17_TI1_RCC_HSE1MHZ) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM17_Init 2 */
 
 /* USER CODE END TIM17_Init 2 */
 
}

I've tested this for TIM16 and TIM17 which show the same behaviour.

This topic has been closed for replies.

3 replies

Nesrine.JLASSI
Visitor II
Apr 16, 2020 8:46 AM UTC

Hi @rb1​ 

Could you please share your .ioc file to check the issue.

Best regards,

Nesrine

rb1
rb1Author
Associate II
Apr 16, 2020 8:52 AM UTC

Hi @Nesrine.JLASSI​ 

Sure.

Nesrine.JLASSI
Visitor II
Apr 16, 2020 12:53 PM UTC

Hello @rb1​ 

Thanks for your feedback, issue confirmed, it will be internally fixed.

Best Regards,

Nesrine