Skip to main content
Noëlie_Jestin
Associate
February 27, 2026
Solved

CubeMX generates incorrect init order for USB PCD + USBX Device

Hello I found this issue, I drop you my report (with IA helping to write it :) )

**Component/Tool:** STM32CubeMX (code generation)

**MCU:** STM32C071KBT3 (STM32C0 family)

**FW Package:** STM32Cube FW_C0 V1.4.0

**Configuration:** USB Device with USBX CDC-ACM class, bare-metal (no RTOS / no ThreadX)

**Description:**

When generating code for a USB Device project using USBX middleware (CDC-ACM class) in bare-metal mode (without RTOS), STM32CubeMX generates the peripheral initialization calls in `main()` in the wrong order:

Generated code (incorrect):

MX_USB_PCD_Init(); // Called FIRST
MX_USBX_Device_Init(); // Called SECOND

**Expected code (correct):**

MX_USBX_Device_Init(); 
MX_USB_PCD_Init(); 

**Root cause analysis:**

`MX_USBX_Device_Init()` calls `ux_system_initialize()` and `ux_device_stack_initialize()` which set up the USBX system memory and device stack. The `MX_USB_PCD_Init()` function's USER CODE section then calls `_ux_dcd_stm32_initialize()` which registers the STM32 DCD driver with the USBX device stack.

If `MX_USB_PCD_Init()` is called before `MX_USBX_Device_Init()`, the USBX system and device stack are not yet initialized when `_ux_dcd_stm32_initialize()` attempts to register with them. This results in USB enumeration failure — the device is not recognized by the host.

**Impact:** USB communication completely non-functional with the generated init order. The device does not enumerate on the USB bus.

**Workaround:** Manually reorder the calls in a `USER CODE BEGIN 2` section, calling `MX_USBX_Device_Init()` before `MX_USB_PCD_Init()`. However this workaround is fragile as CubeMX re-generation can overwrite the auto-generated init order section and reintroduce the bug.

**Steps to reproduce:**
1. Create a new STM32CubeMX project for STM32C071KBT3
2. Enable USB in Device mode
3. Add USBX middleware with CDC-ACM class
4. Configure for bare-metal (no RTOS)
5. Generate code
6. Observe that `MX_USB_PCD_Init()` is placed before `MX_USBX_Device_Init()` in the generated `main()` function

**Expected fix:** CubeMX code generator should place `MX_USBX_Device_Init()` before `MX_USB_PCD_Init()` in the generated initialization sequence when USBX middleware is enabled.


Edited to apply proper source code formatting - please see How to insert source code for future reference.

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
February 27, 2026

Hello @Noëlie_Jestin 

Your detailed explanation is much appreciated.

I totally agree with you , actually after checking the  Ux_Device_CDC_ACM example , the order should be as you mentioned , issue has been escalated to dev team under internal ticket ID 0060181.

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1 reply

Ghofrane GSOURI
Ghofrane GSOURIBest answer
ST Technical Moderator
February 27, 2026

Hello @Noëlie_Jestin 

Your detailed explanation is much appreciated.

I totally agree with you , actually after checking the  Ux_Device_CDC_ACM example , the order should be as you mentioned , issue has been escalated to dev team under internal ticket ID 0060181.

I will keep you posted with updates.

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.