Skip to main content
Associate
February 17, 2025
Solved

CubeMX feature request: useful error message on invalid pin-ioc.cfg

I made a change to my project (using an STM32H7S3L8 part), saved the results, and a few days later tried to reload the project, but got a "Not a valid ioc file" error message.  Here is the output of the log file:

```

2025-02-17 10:59:38,352 [FATAL] ProjectFactory:568 - Exception caught
java.lang.NumberFormatException: For input string: ""
at java.lang.NumberFormatException.forInputString(NumberFormatException.java:67) ~[?:?]
at java.lang.Long.parseLong(Long.java:719) ~[?:?]
at java.lang.Long.valueOf(Long.java:1157) ~[?:?]
at com.st.microxplorer.mcu.memorymap.MemInfoExtractor$ETHInfoExtractor.onETHEnable(MemInfoExtractor.java:4561) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.memorymap.MemInfoExtractor.completInit(MemInfoExtractor.java:252) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.memorymap.MemoryMapService.MMTActivated(MemoryMapService.java:1259) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.memorymap.MemoryMapService.loadConfigV3(MemoryMapService.java:2578) ~[STM32CubeMX:?]
at com.st.microxplorer.mcu.Mcu.loadConfProperties(Mcu.java:6750) ~[STM32CubeMX:?]
at com.st.microxplorer.mxsystem.ProjectFactory.swingWorkerLoad(ProjectFactory.java:494) ~[STM32CubeMX:?]
at com.st.microxplorer.util.ProcessBarDialog.performAction(ProcessBarDialog.java:86) ~[STM32CubeMX:?]
at com.st.microxplorer.util.ProcessBarDialog$1.doInBackground(ProcessBarDialog.java:157) ~[STM32CubeMX:?]
at com.st.microxplorer.util.ProcessBarDialog$1.doInBackground(ProcessBarDialog.java:154) ~[STM32CubeMX:?]
at javax.swing.SwingWorker$1.call(SwingWorker.java:305) ~[?:?]
at java.util.concurrent.FutureTask.run(FutureTask.java:317) ~[?:?]
at javax.swing.SwingWorker.run(SwingWorker.java:342) ~[?:?]
at java.util.concurrent.ThreadPoolExecutor.runWorker(ThreadPoolExecutor.java:1144) ~[?:?]
at java.util.concurrent.ThreadPoolExecutor$Worker.run(ThreadPoolExecutor.java:642) ~[?:?]
at java.lang.Thread.run(Thread.java:1583) ~[?:?]

```

It would be rather useful to tell me which key had the problem so that I could edit the file in vim (at least enough to bring the tool up).  (This is independent of the tool writing a file that it later could not read, but I don't have the information on which change that I made that tickled that bug.)  This issue is occurring on CubeMX v6.13.0.

This topic has been closed for replies.
Souhaib MAZHOUDBest answer
ST Technical Moderator
February 18, 2025

Hello @sf_it 

Actually, this is a known issue with the STM32CubeMX 6.13 version which occurs when activating the memory mapping tool (MMT) and Ethernet.

As a temporary workaround, you can open the IOC by following these steps:
- Open the IOC file with a text editor
- Delete all references to "MMTAppReg"
- Modify "MMTAppRegionsCount" to "MMTAppRegionsCount=0"
- Reopen the IOC file with STM32CubeMX 6.13.0

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

3 replies

Pavel A.
February 17, 2025

> at com.st.microxplorer.mcu.memorymap.MemInfoExtractor$ETHInfoExtractor.onETHEnable(

This hints to something related to ETH.

Generally, if something worked before and makes trouble now - use your version control (git or whatever) and roll back to happiness.

 

sf_itAuthor
Associate
February 18, 2025

Yes, that was obvious.  Unfortunately, the number of lines changed were quite numerous -- to the point that I'm abandoning CubeMX as the tool.

Souhaib MAZHOUDBest answer
ST Technical Moderator
February 18, 2025

Hello @sf_it 

Actually, this is a known issue with the STM32CubeMX 6.13 version which occurs when activating the memory mapping tool (MMT) and Ethernet.

As a temporary workaround, you can open the IOC by following these steps:
- Open the IOC file with a text editor
- Delete all references to "MMTAppReg"
- Modify "MMTAppRegionsCount" to "MMTAppRegionsCount=0"
- Reopen the IOC file with STM32CubeMX 6.13.0

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.