Skip to main content
Wde G.1
Associate II
May 7, 2020
Question

CubeMX doesn't allow Fadc > 18 MHz for H743 Rev. V

  • May 7, 2020
  • 1 reply
  • 678 views

If from the "Clock Configuration" tab Fadc > 36Mhz then the Clock prescaler for the ADC is automatically set to /2 where the /1 is diabled. For > 72MHz it is /4 where /1 and /2 are disabled. Rev. 2 has an additional /2 divider that has been taken into account in the HAL code but not in CubeMX I assume.

Code snippet from stm32h7xx_hal_adc.c:

/**

 * @brief Configure boost mode of selected ADC.

 * @note  Prerequisite condition to use this function: ADC conversions must be

 *     stopped.

 * @param hadc ADC handle

 * @retval None.

 */

void ADC_ConfigureBoostMode(ADC_HandleTypeDef* hadc)

 else /* STM32H7 silicon Rev.V */
 {
 freq /= 2U; /* divider by 2 for Rev.V */
 
 if (freq <= 6250000UL)
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, 0UL);
 }
 else if(freq <= 12500000UL)
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, ADC_CR_BOOST_0);
 }
 else if(freq <= 25000000UL)
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, ADC_CR_BOOST_1);
 }
 else /* if(freq > 25000000UL) */
 {
 MODIFY_REG(hadc->Instance->CR, ADC_CR_BOOST, ADC_CR_BOOST_1 | ADC_CR_BOOST_0);
 }
 }
#endif /* ADC_VER_V5_3 */
}

This topic has been closed for replies.

1 reply

Khouloud ZEMMELI
ST Employee
November 30, 2020

Hi @Wde G.1​ 

Can you please check with the latest CubeMX version (6.1.0) ? the problem related to "Clock Prescaler divided by 1 always grayed" was fixed.

Thanks, Khouloud