Skip to main content
matt-crc
Senior III
Mar 8, 2025 8:33 PM UTC
Question

CubeMx does not configure FileX properly - Bugs

There are 3 bugs reported here:

Bug 1:

In the FileX parameters GUI, under SRAM Disk Driver: The range for the "SRAM Disk Size" is wrong.  The Address space allows for 256MBytes, not 256KBytes.

mattcrc_0-1741464093433.png

Workaround - After CubeMX regenerates the code, I have to change the #define manually in the code.

Seems to work on my board with 64Mb, (in the example below I have the base address set to C0200000 and using the upper 32MB)

mattcrc_2-1741464364746.png

Bug-2

Under "Software Packs", when we select "LevelX NOR custom inferface", CubeMX doesn't seem to do anything.  We are unable to select the "File System Interface" in the parameters table:

mattcrc_3-1741464726324.png

If you unselect the LevelX QuadSPI memory interface,

mattcrc_4-1741464889996.png

The majority of the configuration parameters in LevelX disappear, but is left with an unselectable option (MT25TL01G

mattcrc_5-1741464993665.png

Bug-3

Since the Custom driver option does not work in CubeMX, we tried to modify the QSPI driver with the MT25TL01G component.  The problem is there are no    " USER COMMENT" sections in the entire file, so we have to make the changes each time CubeMX runs.  We have it working, but CubeMX shouldn't be overwriting code all the time.  There needs to be a way for CubeMX to exclude certain files from updating. - OR - make sure each file has a "USER COMMENT" and the very  beginning and end of each file, so users can comment out all the CubeMX code between the comment sandwich....

mattcrc_7-1741465761116.png

 

 

9 replies

matt-crc
matt-crcAuthor
Senior III
Mar 8, 2025 8:37 PM UTC

Hello ST employee,

I bet you will ask me for the .ioc file... so here it is.

Ghofrane GSOURI
ST Technical Moderator
Mar 10, 2025 11:23 AM UTC

Hello @matt-crc 

First let me thank you for posting.

I'm currently investigating this, I will get back to you asap

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Ghofrane GSOURI
ST Technical Moderator
Mar 11, 2025 8:22 AM UTC

Hello @matt-crc 

Regarding the first bug : 

The STM32H7 series typically offers up to 1 MB of RAM, not 256 MB, which is a much larger memory size 

Clarification on RAM Size :

Actual RAM Size: The STM32H7 series includes devices with up to 1 MB of RAM, divided into different types such as 192 Kbytes of TCM RAM (inc. 64 Kbytes of ITCM RAM +128 Kbytes of DTCM RAM for time critical routines), Up to 864 Kbytes of user SRAM, and 4 Kbytes of SRAM in Backup domain

GhofraneGSOURI_0-1741680777372.png

The mention of a 256 MB address space is likely incorrect for the internal SRAM of the STM32H7. This could be a mix-up with external memory configurations or a misunderstanding of how memory is allocated in the system.

External Memory: If you are using external memory like SDRAM, you might be able to configure a larger address space, but this would require specific hardware and configuration beyond the standard STM32H7 setup7.

 

Regarding the second bug :

Under "Software Packs", when we select "LevelX NOR custom inferface"
CubeMX add the following define

--> In FileX\Target\fx_stm32_levelx_nor_driver.h
#define LX_NOR_CUSTOM_DRIVER

Regarding the third bug : still under investigation

 

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
matt-crc
matt-crcAuthor
Senior III
Mar 11, 2025 1:47 PM UTC

Hi @Ghofrane GSOURI 

First bug report

I find your first answer strange because you do not limit the size of the drive when using external FLASH, but you limit the size of  the drive when using external RAM.  The data sheet that you provided only says there is 2MB of flash in the chip, yet I can define a 128MB flash drive.  I would have assumed that ST would use the same logic for external RAM.

Second bug report

there doesn't seem to be a #define LX_NOR_CUSTOM_DRIVER in my file.

mattcrc_0-1741700710799.png

 

ofer-bahar
Associate II
Jun 9, 2026 9:36 AM UTC

ST has MAJOR problems with FILEX which it does not disclose to its users most likely !!!

e.g. STM32 CubeIDE 2.1.1 with STM32 Cube MX 6.16.1

  1. THE FILEX INCLUSION DOES NOT GENERATE THE CODE IN THE CORRECT PLACE
  2. THE FILEX INCLUSION REMOVES HAL DRIVERD DIRECTOTY FROM THE PROJECT 

VERY BAD VERY BAD 

ST - WHY DON’T YOU DISCLOSE THE PROBLEMS YOU HAVE THERE AND LET YOUR USER WRITE CODE INSTEAD OF FIGHTING YOU TOOLS !!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!

Ghofrane GSOURI
ST Technical Moderator
Jun 9, 2026 10:00 AM UTC

Hello ​@ofer-bahar 

Could you please provide additional details about the issue?
More specifically, when you say that FileX inclusion does not generate the code in the correct place, please indicate the actual location where the code is generated and the location where you expect it to be generated.

If possible, please also share the .ioc file for further analysis.

Please note that the latest version of STM32CubeMX is 6.17.0

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ofer-bahar
Associate II
Jun 9, 2026 11:13 AM UTC

Hi Ghofrane

attached is the ioc

the problem of the code generation was verified by mw TWICE, and I also found some workaround for this

basically the problems are

  1. generation create “middleware\..\...” at the wrong location of the project which is not included at all, and has to be copied manually into either Appli or FSBL
  2. sometime without any relation to FILEX, but as long as the FILEX is checked in the MX, and something else is modified/added/removed , the whole drivers folder of the project is GONE !!

For now, my workaround is copy the whole FileX folders to my project and not including it at all in the MX, so this is how it works now (for me)

 

Regards

Ofer

ofer-bahar
Associate II
Jun 9, 2026 5:38 PM UTC

HI AGAIN ST

I think you know why you suggested me to use MX 6.17.0 

BECAUSE MX6.16 HAS MANY MORE BUGS    !!!!

NOW I SEE THAT THE RIF GENERATION IN APPLI DOES NOT COPY THE stm32n6xx_hal_rif.c to the APPLI project 

and until I copy it MANUALLY - IT DOES NOT WORK (obviously !!!!)

SO - ST - WOULD YOU LIKE TO SAY THE WHOLE STORY ABOUT THE MMX 6.16 ????  

OR LET YOUR USERS FIGHT for nothing 

TDK
Jun 9, 2026 7:56 PM UTC

Who’s fighting for nothing? What does that entail exactly?

As new versions are released, they will contain fixes for bugs in previous releases. That is expected, and desired. Release notes and Errata notes exist if you wish to see what is solved and what is not solved and known about. There is no grand conspiracy here.

N6 is unique and FileX is not terribly commonly used so expect to use some problem solving skills. If needing to copy files is the biggest hurdle you’re coming across in your work, consider yourself lucky.

"If you feel a post has answered your question, please click ""Accept as Solution""."