Skip to main content
Paul Mellor
Associate II
July 4, 2017
Question

CubeMX code for Nucleo32 L432KC does not build

Posted on July 04, 2017 at 18:33

Repro steps...

  • Create a new CubeMX project, selecting the Nucleo32 L432KC board.
  • In settings give it a name and select to generate code for the 'System Workbench for STM32' selecting SW4STM32
  • Generate the code and open the project.
  • The project does not build.

The problem is that core_cm4.h cannot be found - its not present.

Can anyone help?

Paul

#nucleo-l432kc #cubemx #sw4stm32
This topic has been closed for replies.

2 replies

john doe
Senior III
July 5, 2017
Posted on July 05, 2017 at 04:56

while you omit such information from your post, did you try to upgrade anything lately? which version of cube is your repository?

remove the 1.8.0 and 1.8.1 directories and zip files and let it download and patch them again. thats what worked for me.

ST Technical Moderator
July 5, 2017
Posted on July 05, 2017 at 10:06

Hi

Mellor.Paul

,

Make sure that the include paths configured properly into the project from the correct directories.

For more help on this issue, please share your .ioc file and provide more details about the tools (Cubex, SW4STM32) version you have used.

Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks