Skip to main content
Andrew C
Associate III
August 6, 2025
Question

CubeMX and setting analog watchdog

When I try to select which channel gets a watchdog, it only gives me one option on the pull down. Instead, if I want to change the channel, I have to unselect all the ADC channels and make sure that the watchdog intended channel is the first one selected. Is this normal?

 

AndrewC_0-1754488831788.png

From the photo above, only one channel is always available in the pull down.

This topic has been closed for replies.

3 replies

TDK
August 6, 2025

What chip?

"If you feel a post has answered your question, please click ""Accept as Solution""."
Andrew C
Andrew CAuthor
Associate III
August 6, 2025

STM32F413ZHT6

TDK
August 6, 2025

You're only converting a single channel as only "Rank 1" appears in your screenshot. If you add additional conversion ranks for different channels, they will show up as an option. Change Number of Conversions to whatever and configure each rank to a channel.

TDK_0-1754516712287.png

 

If you still can't get it, include your IOC file.

"If you feel a post has answered your question, please click ""Accept as Solution""."