Skip to main content
MForb.1
Associate II
May 18, 2020 8:22 PM UTC
Question

CubeMX and Dropbox: Doesn't work reliably, program usually hangs during code generation

I've noticed an ongoing problem with CubeMX hanging up during code generation. I typically store projects in a Dropbox folder, mirrored onto their cloud service. While the folder is local, it's copied up to the Dropbox servers. Most times, when I try to generate code, CubeMX gets as far as starting to generate user code and set up the folder structure, then hangs forever. I have to invoke Task Manager (I'm on a Win7 box) to force-close the program. Running the same .ioc file in a local temp directory, it works fine. I've tried running CubeMX in administrator mode, with no improvement. This has been an ongoing problem for as long as I've been using CubeMX, at least three years.

This topic has been closed for replies.