Skip to main content
bbee
Senior
Apr 2, 2025 1:23 PM UTC
Solved

CubeMX 6.14 encoding of generated code changed?

Hi,

just made an update of CubeMX from 6.11.1 to 6.14.
The problem I have is that our comments within user blocks were ISO-8859-1 encoded and this never was a problem until now and with 6.14, when we generate code, all Umlauts are replaced with the UTF-8 sequence EF BF BD.

Is there an option to tell CubeMX to use ISO-8859-1 for reading and encoding?

This topic has been closed for replies.
bbee
bbeeBest answer
Senior
Apr 2, 2025 1:57 PM UTC

Nope, as I said, the files are allready ISO-8859-1 encoded before the generation and this wasn't a problem at least until version 6.11.1.
Meanwhile I found a workaround and added the line

-Dfile.encoding=ISO-8859-1

into STM32CubeMX.l4j.ini

Now CubeMX reads and generates the files in the correct encoding again.


3 replies

AScha.3
Super User
Apr 2, 2025 1:34 PM UTC

Hi,

afaik this has not much to do with the CubeMx version, but with the IDE version and especially its settings:

 

AScha3_0-1743600742758.png

...so try:

AScha3_1-1743600794392.png

- but there might be other definitions in the settings and preferences...just look. :)

 

If you feel a post has answered your question, please click on " Best Answer ".
bbee
bbeeAuthorBest answer
Senior
Apr 2, 2025 1:57 PM UTC

Nope, as I said, the files are allready ISO-8859-1 encoded before the generation and this wasn't a problem at least until version 6.11.1.
Meanwhile I found a workaround and added the line

-Dfile.encoding=ISO-8859-1

into STM32CubeMX.l4j.ini

Now CubeMX reads and generates the files in the correct encoding again.


Pavel A.
Apr 2, 2025 8:42 PM UTC

It's the time to move to utf-8, for all tools.