Skip to main content
Adalgiso
Associate III
Sep 13, 2018 8:05 AM UTC
Question

CubeMX 4.26 cannot open migrated project

I migrated CubeMX 4.25 to 4.26.1 and after migrating my project I cannot access the project anymore. I have the sandbox running I can access the generation code (did not try to generate new code).

I have attached the .ioc file.

This topic has been closed for replies.

3 replies

Tomas DRESLER
Associate II
Sep 13, 2018 12:46 PM UTC

Please report via Online support, I can confirm issue loading it into Mx 4.26.1 (no crash, but loading is unfinished).

ST Technical Moderator
Sep 13, 2018 1:58 PM UTC

Hello,

This issue is raised internally to CubeMx team for check. We will come back to you as soon as possible.

Thank you for your contirbution.

With Regards,

Imen.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Jocelyn RICARD
ST Employee
Sep 14, 2018 12:58 PM UTC

Hello,

I answered to your request in online support and answer here to share the information.

This issue is already known and is a regression related to ADC on 4.26.1

It should be solved on release 4.27.

By this time you can use the 4.26.0

Just edit the IOC file to set version to 4.26.0 before that to allow openning of IOC.

Best regards

Jocelyn

Update : The cube MX 4.27 is already available. You can open your project with it :smiling_face_with_smiling_eyes: