Skip to main content
Innomatic
Associate III
Sep 11, 2018 3:46 AM UTC
Question

CubeMX 4.26.1 Makefile project generation bug?

When a TSC is selected, CubeMX populates two lines of the same source file in the Makefile. In other words, there are two lines of:

Drivers/STM32L0xx_HAL_Driver/Src/stm32l0xx_hal_tsc.c

in the Makefile created by CubeMX. To reproduce, create a new project with a L0 device, select TSC with some channel settings, and generate a Makefile project.

Another bug is that CubeMX failed to update existing Makefile. To reproduce this bug, simply open up existing Makefile project file (*.ioc) and try to regenerate it.

This topic has been closed for replies.