Associate III
December 7, 2016
Question
CubeMX 4.18 pegs CPU in Clock Tab on macOS
- December 7, 2016
- 8 replies
- 1351 views
Posted on December 07, 2016 at 16:41
I notice that whenever I am in the Clock Configuration tab of CubeMX 4.18 the CPU activity goes to 100%. This is on macOS 10.12.1 and Java 1.8.0_111. Changing to any other tab reduces CPU to just a few percent. Not a crushing issue but probably not the intended behavior so thought I would mention it.
If it helps, I've attached the project ioc file.
#cubemx #mac-os