Skip to main content
AEfth
Associate II
March 31, 2025
Question

CMake project bug in cubeMX6.14.0

On a NUCLEO-H7S3L8 I've been testing the Projects/NUCLEO-H7S3L8/Applications/USBPD from STM32Cube_FW_H7RS_V1.2.0 with cubeMX6.14.0. I use the VScode extension, so I select the CMake toolchain. I select the "copy only necessary files" in code generation.

I noticed a different behaviour when I just copy the .ioc file from the example (and just select CMake) to when I use the "access to example selector" button of cubeMX. The .ioc file in the example does not specify the specific board: it has board=custom, while the one from the example selector has: BSP_IP_NAME=NUCLEO-H7S3L8 board=NUCLEO-H7S3L8. That is the only difference I see in the .ioc files.

The code generated from either of these does not operate correctly. 

With example selector:

- BSP code is added in the folder and included in CMake files.

- The libraries are not referenced in CMake files. For example, all the *HAL_Driver/Src/* files are missing in set(STM32_Drivers_Src part of mx-generated.cmake. The same holds for all Middleware libraries.

- As a result, the project does not even build.

With copying the .ioc from the example:

- The BSP code is not added in the folder and it is not referenced in the CMake files.

- The libraries, however, are correctly referenced in the CMake files.

- As a result, the project builds, but because the BSP code for the board is missing, it does not work on the board.

There must be a bug somewhere in the code generation script, which does not produce the library references in the CMake files when BSP code is included. I haven't tried on anything other than CMake.

As a workaround, I just build both and then compare all the CMake related files and fix them.

This topic has been closed for replies.

2 replies

ST Technical Moderator
April 18, 2025

Hello @AEfth 

Thank you for your contribution,
The issue is currently under investigation internally.
When you copy the .ioc from the example, you should copy .extSettings file as well that contain the BSP references, could you verify please?

KR,

Souhaib

To give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
AEfth
AEfthAuthor
Associate II
June 15, 2025

Hi,

I've just came back to this now with cubeMX6.14.1. I'm also on Linux, I didn't mention this in the original post.

The situation is unchanged.

When I copy the .extSettings file together with the .ioc file from the example in my downloaded repository, I still get the same behaviour as with the example selector. The BSP files are referenced correctly in Appli/mx-generated.cmake but the source code for the libraries (HAL, Middleware, Utilities for TRACER_EMB) are not referenced. The set(STM32_Drivers_Src part of the file just ends after the BSP source files.

Without .extSettings, Appli/mx-generated.cmake does include all references to the libraries source files, but the BSP files are missing.

Best,

Aris