Skip to main content
Associate
August 11, 2025
Solved

CMake Errors If STM32CubeMX Project Name Contains Spaces

I was following the tutorial (Get started with STM32Cube for VS Code: from installation to debugging - YouTube) when I managed to find a nasty footgun. STM32CubeMx will allow you to create a project whose name contains a space, and then if you set the toolchain to CMake, it generates the code fine, but if you load the project into STM32Cube for VSC and try to build, you will get all kinds of cryptic CMAKE error messages caused by the space in the project name.

Now, STM32CubeMx does have some input validation. It only prevents you from initially generating the project IF you have space in the name and you set the toolchain to CMake BEFORE you generate the code, but that's it. If you save the IOC with a space, save the project as with a space, you generate under any of the other toolchains then switch to CMake, you'll trigger this error.

I burned a few hours on this, so I thought it would be worth bringing up to save someone else the headache in the future. You might want to implement some sort of detection for projects with spaces so you can catch the error early. Given that STM32CubeMx + VSC seems to be the happy path moving forward, I'd also be updating the STM32CubeMx to at a minimum throw an error when generating CMake projects when the name contains a space, and possible enforcing no spaces in project names across all toolchains.

Anyway, in the end I figured out the error and I've got it working on both MacOS and Win11. The integration into VSC is amazing, working very smoothly!

This topic has been closed for replies.
Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
August 19, 2025

thanks @Trev_AU for the headup

STM32CubeMX is not supposed to accept project names containing spaces or special characters when generating a cmake project but seems to bug when saving into a folder with space in the name. 

 

I'm transferring this thread to STM32CubeMX forum to be treated ASAP

5 replies

Andrew Neil
Super User
August 11, 2025
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Trev_AUAuthor
Associate
August 11, 2025

Ha! I know right. I spend a lot of time on the terminal so I'm normally a stickler with trying to avoid any spaces in the path. When you go "Save as" in MX, you pick the folder location, and I happened to pick the my "project folder" which is date prefixed with a space (2025-08-11 Happy project name).

Now this is a quirk of MX. In conflates the "project folder" with the "project name", which I think is derived from the "IOC name". There is some sort of underlying assumption that they are all the same. If you generate a project (without spaces), then copy it to a folder with a space, the code generator works fine (it uses the old project name), somehow it finds the project (even though the projects location + project name != project folder), and this project works fine in CubeMX + VSC. This makes sense as I've copied IOC files around into different projects with no issues previously.

Interestingly it's not the path that is the problem, it's the generated CMAKE variables based on the project name that are mangled. It's blaringly obvious what the problem is, akin to #define with spaces, instead of #define WITHOUT_SPACES. Not an error you'd ever made if you typed it, but the code generator will happily spit it out.

I'm just trying to save someone (let's face it, me in 6 months), the hassle of figuring out why their project won't build over a simple code gen error that is fairly simple to detect.

Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
August 19, 2025

thanks @Trev_AU for the headup

STM32CubeMX is not supposed to accept project names containing spaces or special characters when generating a cmake project but seems to bug when saving into a folder with space in the name. 

 

I'm transferring this thread to STM32CubeMX forum to be treated ASAP

ST Technical Moderator
August 19, 2025

Hello @Trev_AU ,

 

Let me thank you for posting and welcome to the ST Community.

I am currently investigating your request, and I will get back to you ASAP.

 

Thanks.

Mahmoud

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ST Technical Moderator
August 19, 2025

Hello @Trev_AU ,

 

Thank you very much for bringing this issue to our attention.

Ticket 215923 has been escalated to the development team for resolution.

 

Thanks.

Mahmoud

 

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.