Skip to main content
nbobovnikov
Associate
Oct 20, 2017 12:51 PM UTC
Question

Change _Error_Handler() function signature

Posted on October 20, 2017 at 14:51

Hello!

Right now CubeMX generates code with the following signature of Error_Handler function:

void

_Error_Handler

(

char

*,

int

);

When I turn my project to use c++, compiler doesn't like it, and I change it to the following:

void

_Error_Handler

(

const

char

*,

int

);

So I suggest to adjust code generation accordingly.

Regards, 

Nikolay

#cubemx #stm32 #code-generation
This topic has been closed for replies.

1 reply

Jeanne Joly
Associate
Feb 8, 2018 4:11 PM UTC
Posted on February 08, 2018 at 17:11

Hello,

Sorry for my late reply.

There are already some threads on that topic. please have a look for instance to this one

https://community.st.com/0D50X00009Xkdm6SAB

.

We do understand the need for you to generate C++project and this need is well known internally.

However, for the moment, with the success of STM32CubeMX, we have a lot of requests/suggestions to study andmanyimprovements to integrate.

And the C++ generation project item is not yet under study currently.

Sorry, for the inconvenience it may cause.

BR. Jeanne