Skip to main content
JVan .3
Associate II
August 27, 2025
Solved

Cannot enable SMPS STM32U385RGT6Q

The new version of CubeMx (6.15.0) nags me about enabling SMPS mode, and I would like to, but the tool seemingly does not have the capability to do so.

Under PWR->Low Power there's a checkbox for "Power Savings Mode" which other forum posts led me to believe would need to be enabled. I have found two things about this checkbox. 1.) It is already enabled and 2.) You cannot disable it.

Then, under "System Core" -> RCC ->Parameter Settings, there's a "Supply Source" parameter. It has only a "PWR_LDO_SUPPLY" option, and cannot be changed to any other value.

Am I missing something here, or is the tool broken?

 

jerry65Best answer
Explorer
September 4, 2025

Hi JVan,

You're not missing anything — CubeMX 6.15.0 currently has a limitation or bug that prevents selecting PWR_SMPS_SUPPLY as the supply source for the STM32U385RGT6Q, even though the hardware supports it. The RCC supply source field is locked to PWR_LDO_SUPPLY, and there's no UI option to change it, which effectively blocks enabling SMPS via CubeMX.

The workaround right now is to manually configure the supply mode in your own code after CubeMX generates the project. You can use HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY); early in main() or before clock config. Just make sure your power configuration and regulators are wired appropriately on your board (SMPS capacitor, voltage ranges, etc.) or it might cause startup failures.

ST likely needs to patch this in a future CubeMX update — report it if you haven’t already. Until then, CubeMX can’t fully configure SMPS mode for STM32U3 chips, and you’ll have to do it manually.

Regards

6 replies

ST Technical Moderator
August 27, 2025

Hello @JVan .3 

This is known issue reported in this post: STM32U3: Missing SMPS in power supply source, and escalated in the Internal ticket number: 214214.

This issue will be fixed in the coming release of CubeMX.

Thank you for your contributions.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
JVan .3
JVan .3Author
Associate II
August 27, 2025

Okay, great and thank you!

 

jerry65Best answer
Explorer
September 4, 2025

Hi JVan,

You're not missing anything — CubeMX 6.15.0 currently has a limitation or bug that prevents selecting PWR_SMPS_SUPPLY as the supply source for the STM32U385RGT6Q, even though the hardware supports it. The RCC supply source field is locked to PWR_LDO_SUPPLY, and there's no UI option to change it, which effectively blocks enabling SMPS via CubeMX.

The workaround right now is to manually configure the supply mode in your own code after CubeMX generates the project. You can use HAL_PWREx_ConfigSupply(PWR_SMPS_SUPPLY); early in main() or before clock config. Just make sure your power configuration and regulators are wired appropriately on your board (SMPS capacitor, voltage ranges, etc.) or it might cause startup failures.

ST likely needs to patch this in a future CubeMX update — report it if you haven’t already. Until then, CubeMX can’t fully configure SMPS mode for STM32U3 chips, and you’ll have to do it manually.

Regards

KDJEM.1
ST Technical Moderator
December 1, 2025

Hello @JVan .3 , @jerry65 and @ShawnLyu ;

 

The issue is fixed in STM32CubeMX 6.16.0 version.

 

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.