Skip to main content
PPopo.1
Senior
Apr 11, 2023 8:59 AM UTC
Question

Can't open .ioc file

I get an error when trying to open .ioc file of the project. It was working fine and i am pretty sure I haven't changed anything about it. Just can't open it anymore for some reason. Also the name that it says that is the right one, is the same as the name of my file.

The error I get:

Invalid Input: Must be project's active .ioc file.

Project's 'camera_module' active one is 'camera_module.ioc' file

This topic has been closed for replies.

1 reply

Ghofrane GSOURI
ST Technical Moderator
Apr 11, 2023 10:30 AM UTC

Hello @PPopo.1​ 

First let me thank you for posting .

Here are a few steps you can try to resolve this issue:

  1. Double-check that the .ioc file you are trying to open is the correct one for your project. It's possible that you may have inadvertently created a duplicate file or renamed the original file.
  2. Make sure that the .ioc file you are trying to open is located in the correct directory for your project. If the file has been moved or saved in a different location, it may not be recognized as the active file.
  3. Try to create a new .ioc file and import your old ioc into it.
  4. If you are still experiencing issues, try restarting your computer and opening the .ioc file again. Sometimes, a simple restart can resolve issues with file recognition.

Thx

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.