Skip to main content
Akash_k
Associate III
Nov 9, 2019 11:38 AM UTC
Question

Can I send and receive data directly using HAL ETH functions without enabling LWIP? If yes, can anyone provide a sample code for the same? What software can I use to check the data transmission and reception ?

I am using NUCLEO-H743ZI2 and STM32CubeMX embedded firmware v1.5.0 .

This topic has been closed for replies.

1 reply

Pavel A.
Nov 9, 2019 9:25 PM UTC

> Can I send and receive data directly using HAL ETH functions without enabling LWIP?

Yes, just take one of LwIP examples without RTOS, and remove LwIP

> What software can I use to check the data transmission and reception ?

LwIP. Put it back =)

The Cube examples come with UDP & TCP echo tool.

-- pa