Skip to main content
DSchm.3
Associate
October 29, 2024
Solved

Bugs in CubeMX 6.12 with new STM32C071 controller

Hello everyone,
we are currently developing a new product based on the new STM32C071G8U. Unfortunately, we found some Bugs in the CubeIDE 16.1 CubeMX extension when configuring the peripheral of the microcontroller.

1. All Packages smaller than 48 pins are missing the HSE oscillator option. According to the datasheet, it should be possible to route the HSE to the OSCX pins. You can also verify this overwriting the automatically generated code to force the use of the HSE. 

DSchm3_0-1730185764666.png

2. The settings in the clock configuration aren't applied and always default to divide by 1.

DSchm3_1-1730185934524.png

3. The STM32C071G8 has only 64 kB of flash, but the automatically generated linker script defines the flash size as 128 kB.

DSchm3_2-1730186088139.png

It would be nice if you could address these bugs in your next software version.

Kind regards
Dominik Schmid

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
October 29, 2024

Hello @DSchm.3 ,

Thank you for having reported.

Looks like you are right. I escalated the issues to our CubeMX teams for analysis via an internal ticket number: 195279.

 I will keep you informed about updates.

(PS: ticket number: 195279 is an internal tracking number and is not accessible or usable by customers).

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

2 replies

Imen.DBest answer
ST Technical Moderator
October 29, 2024

Hello @DSchm.3 ,

Thank you for having reported.

Looks like you are right. I escalated the issues to our CubeMX teams for analysis via an internal ticket number: 195279.

 I will keep you informed about updates.

(PS: ticket number: 195279 is an internal tracking number and is not accessible or usable by customers).

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
ST Technical Moderator
November 6, 2024

Hi @DSchm.3 ,

Issues are confirmed by CubeMx team and will be fixed in the coming releases.

Thank you for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks