Skip to main content
KnarfB
Super User
June 4, 2023
Question

Bug: STM32CubeMX: Project Manager > Project > Firmware Relative Path - Cannot enter a *relative* path

In STM32CubeMX 6.8.1. (and before), there is an option to enter a custom path to the firmware. But, in contrast to what it says, I can only pick an absolute path here. This is unwanted when projects are shared between users/machines. For example, I would like to store the firmware in the same git repository as a number of projects using it. Workaround: patching the generated Makefiles :(

KnarfB

This topic has been closed for replies.

1 reply

Pavel A.
June 4, 2023

This is a well known limitation, usually people find some workaround that works for them.

For example you can choose a single fixed location outside of any user profile (such as /opt/st/...)

You can also create symlinks to the Cube firmware location in your projects, and/or use environment variables.