Skip to main content
Hector Fernandez
Associate II
April 12, 2018
Question

Bug report STM32CubeMX 4.25.0: RCC_OscInitStruct.PLL.PLLM

Posted on April 12, 2018 at 12:55

I am using a 

http://www.st.com/en/evaluation-tools/b-l475e-iot01a.html

 with STM32L475VGTx. When I generate the source code with STM32CUBEMX 4.25.0 and STM32Cube FW_L4 V1.11.0, i noticed that inside SystemClock_Config() in main.c, the following line of code is not used:

   RCC_OscInitStruct.PLL.PLLM = 1;

So, my USB peripheral doesn't work because USB must be configured to 48Mhz. But if this line of code is not called, the USB frequency is wrongly-configured. But when I add manually this line (and the correct value), USB peripheral works perfectly.

This bug appears in new

STM32Cube projects as well as migrated ones.

I have checked other projects made using

STM32CUBEMX

 4.24.0 and that line of code is not missing.

#cpu-clock-frequency #stm32cube #stm32cubemx-4.25.0 #bug-report
This topic has been closed for replies.

5 replies

Nawres GHARBI
ST Technical Moderator
April 18, 2018
Posted on April 18, 2018 at 11:39

Hi Hector, 

We are already fixing this issue and it will be delivered in the next release of CubeMX. 

As a workaround you can generate the RCC configuration using the LL driver where the PLLM is well configured. 

thanks for using STM32CubeMX

Nawres GHARBI
ST Technical Moderator
May 7, 2018
Posted on May 07, 2018 at 09:59

The 4.25.1 will be available this week fixing this issue 

Stay tuned

Yanmin Huang
Visitor II
May 21, 2018
Posted on May 21, 2018 at 06:59

Hi,

I did not see 4.25.1 generate pllm line.

Did I do something wrong?

thanks.