Skip to main content
Sidlauskas.David
Associate III
Mar 17, 2018 8:08 PM UTC
Question

Bug Report: CubeMX Generates Bad Init Code

Posted on March 17, 2018 at 21:08

Using CubeMX V4.7.25.0 I get initialization code for RTC.c that won't compile when I request initialization be generated as .c.h file pairs.

Simple demo case:

Start CubeMX

New Project

Select STMf103C8Tx as target

Under Pins Select RTC-> Activate Clock Source.

Under Project settings:

   Project Name: Test

   Location: C:\Temp\

   Under Code Generator Tab:

         Check Generate peripheral initialization as pair of .c/.h files

Generate code for TrueStudio

When I build the generated code I get the following errors:

..\..\..\Src\rtc.c:73:5: warning: implicit declaration of function 'LL_PWR_EnableBkUpAccess' [-Wimplicit-function-declaration] LL_PWR_EnableBkUpAccess();..\..\..\Src\rtc.c:75:5: warning: implicit declaration of function 'LL_APB1_GRP1_EnableClock' [-Wimplicit-function-declaration]  LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP);..\..\..\Src\rtc.c:75:30: error: 'LL_APB1_GRP1_PERIPH_BKP' undeclared (first use in this function)

     LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP);

                            

If I generate code for the test project with the peripheral inits in main(), the project will then build without error.

Is this a CubeMx bug?

Dave

#cubemx-bug-init.-code
This topic has been closed for replies.

3 replies

imi415
Associate
Mar 18, 2018 2:48 PM UTC
Posted on March 18, 2018 at 15:48

As a temporary workaround, I replaced these lines with which generated by older version of CubeMX.

However, this will be replaced back by CubeMX after re-generation.

LL_PWR_EnableBkUpAccess

();

/* Enable BKP CLK enable for backup registers */

LL_APB1_GRP1_EnableClock

(LL_APB1_GRP1_PERIPH_BKP);

Replaced with:

HAL_PWR_EnableBkUpAccess

();

/* Enable BKP CLK enable for backup registers */

__HAL_RCC_BKP_CLK_ENABLE

();

Sergey Starovoitov
Associate
Jun 5, 2018 4:00 PM UTC
Posted on June 05, 2018 at 16:00

 ,

 ,

I put this code into the user code section before the problem code to avoid the CubeMX code replacement:

♯ warning These definitions is a temporary workaround. Remove them, when the STM32CubeMX bug will be fixed.

 ,

♯ define LL_PWR_EnableBkUpAccess() HAL_PWR_EnableBkUpAccess()

 ,

♯ define LL_APB1_GRP1_EnableClock(LL_APB1_GRP1_PERIPH_BKP) __HAL_RCC_BKP_CLK_ENABLE()
ST Technical Moderator
Mar 22, 2018 2:25 PM UTC
Posted on March 22, 2018 at 15:25

Hello,

This is knownissue already reported to CubeMx team for fix.

https://community.st.com/0D50X00009XkWuZSAV

Sorry for the inconvenience it may bring.

Kind Regards,

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks