Skip to main content
frackers
Senior
Jan 12, 2017 12:57 AM UTC
Solved

Bug Report: CUBEMX 4.18.0 no trigger selection on ADC

Posted on January 12, 2017 at 01:57

Upgrading from 4.17 to 4.18 has silently removed the selection of external triggers from ADC2 on an F303RE. Not only are the selections missing from the generated code, the option in the UI is missing as well.

Manually patching the generated 'main.c' file fixes the problem but it means that each time I regenerate the code I have to remember to hack it.

I would also question the operation of the EOCSelection field as the UI allows 'ADC_EOC_SINGLE_SEQ_CONV' to be chosen but the HAL code itself says '/*!< reserved for future use */'

#cubemx #adc
This topic has been closed for replies.
Jeanne Joly
Jeanne JolyBest answer
Associate
Feb 9, 2017 4:09 PM UTC
Posted on February 09, 2017 at 17:09

Hello

Gilks.Robin

,

The issue you highlighted willl be fixed in the next release (CubeMX4.20).

BR. Eric

3 replies

ST Technical Moderator
Jan 13, 2017 2:14 PM UTC
Posted on January 13, 2017 at 15:14

Hello

Gilks.Robin

,

Your issue is reported internally to our CubeMx team for checking & come back to you.

Thank you for your feedback.

Regards

ImenD

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Jeanne Joly
Associate
Jan 17, 2017 8:51 AM UTC
Posted on January 17, 2017 at 09:51

Hello

Gilks.Robin

,

Thanks for your post.

Regarding your first point towards the external triggers, you are right, this issue will be normally delivered in the next CubeMX release. It was a mistake.

For your second point regarding

ADC_EOC_SINGLE_SEQ_CONV, it is a feature possible on HW side but, since a couple of years, we did not findany use case in SW in the HAL driver. We use eitherADC_EOC_SINGLE_CONV orADC_EOC_SEQ_CONV. With your post, as this variable is not use, we decided to delete this variable. It will be as well available in the nextCubeMX release.

BR. Eric

Jeanne Joly
Jeanne JolyBest answer
Associate
Feb 9, 2017 4:09 PM UTC
Posted on February 09, 2017 at 17:09

Hello

Gilks.Robin

,

The issue you highlighted willl be fixed in the next release (CubeMX4.20).

BR. Eric