Senior III
October 28, 2025
Question
BUG: MX-cube / Cube-IDE goes into an infinite loop and corrupts the .ioc file
- October 28, 2025
- 3 replies
- 300 views
When I try and enable UART5 in the .n657_dk2.ioc file, the development system seems to go into an infinite loop with the mouse cursor spinning endlessly.
Bug1: To replicate,
1- open the n657_dk2.ioc file
2- goto the connectivity section
3- enable UART5 in FSBL
4- change mode to Asynchronous
5- set Hardware Flow control to RTS/CTS.
system hangs....
Bug 2: if you try and save the file, it corrupts the file and you cannot edit the .ioc file anymore.
.ioc file attached
IMPORTANT!!! I need a fast work around so I can go to layout this week....