Bug in CubeMX with FATFS on SD-Card and FreeRTOS
- 5 replies
- 3145 views
The MX_FATFS_Init function is beeing called in the main function and again in the default task. After the second call the SD_Path is invalid. I'm using CubeMX 4.13.0 with the STM32F417IGH6, the configuration is in the attachments.
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_DMA_Init();
MX_SDIO_SD_Init();
MX_FATFS_Init();
...
/* StartDefaultTask function */
void StartDefaultTask(void const * argument)
{
/* init code for FATFS */
MX_FATFS_Init();
/* USER CODE BEGIN 5 */
/* Infinite loop */
for(;;)
{
osDelay(1);
}
/* USER CODE END 5 */
}
#bug #cubemx