Skip to main content
Senior
Oct 19, 2019 12:26 PM UTC
Question

[BUG] FreeRTOS/LwIP thread priority range for TCPIP_THREAD_PRIO, DEFAULT_THREAD_PRIO and SLIPIF_THREAD_PRIO in CubeMX wrong

Hello,

I think the correct range for TCPIP_THREAD_PRIO, DEFAULT_THREAD_PRIO, SLIPIF_THREAD_PRIO and possible others in CubeMX LWIP configuration should be -3 to +3 and not 0 to 6.

And the default value should be lower than 3 (osPriorityRealtime) definitely to avoid conflicts with low level ETH send/receive threads.

This topic has been closed for replies.

1 reply

SStorAuthor
Senior
Jan 9, 2020 2:36 PM UTC

Ok, the issue seems to been fixed since new CubeMX 5.5.0, at least for TCPIP_THREAD_PRIO in generated file lwipopts.h

/*----- Value in opt.h for TCPIP_THREAD_PRIO: 1 -----*/
#define TCPIP_THREAD_PRIO osPriorityNormal
 
/*----- Value in opt.h for SLIPIF_THREAD_PRIO: 1 -----*/
#define SLIPIF_THREAD_PRIO 3
 
/*----- Value in opt.h for DEFAULT_THREAD_PRIO: 1 -----*/
#define DEFAULT_THREAD_PRIO 3

Now a value of 3 in CubeMX is interpreted as osPriorityNormal (0) correctly 

typedef enum {
 osPriorityIdle = -3, ///< priority: idle (lowest)
 osPriorityLow = -2, ///< priority: low
 osPriorityBelowNormal = -1, ///< priority: below normal
 osPriorityNormal = 0, ///< priority: normal (default)
 osPriorityAboveNormal = +1, ///< priority: above normal
 osPriorityHigh = +2, ///< priority: high
 osPriorityRealtime = +3, ///< priority: realtime (highest)
 osPriorityError = 0x84 ///< system cannot determine priority or thread has illegal priority
} osPriority;

Could you check if the same issue also matches the interpretation for SLIPIF_THREAD_PRIO and DEFAULT_THREAD_PRIO? 

Thank you for your efforts!