Skip to main content
Phanirajkiran M
Senior
May 16, 2018 2:13 PM UTC
Solved

BUG CubeMX for Nucleo L4R5ZI

Posted on May 16, 2018 at 16:13

Hi CUBEMX Team,

for NucleoL4R5ZI 

LPUART1 is taking as GPIOC port. 

It has to be GPIOG port. 

0690X0000060KdkQAE.png

Please fix this 

Thanks

Phanirajkiran

#cubemx #bug
This topic has been closed for replies.
Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
May 21, 2018 9:10 AM UTC
Posted on May 21, 2018 at 11:10

Hi 

Phanirajkiran, 

When loading the board, please select init peripherals and the LPUART will be at the right port. 

Enabling manually the peripheral will select the first available port and not the dedicated one on the board

4 replies

ST Technical Moderator
May 16, 2018 2:58 PM UTC
Posted on May 16, 2018 at 16:58

Hello

phanirajkiran.ma

,

Which CubeMx version are you using?

With Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Phanirajkiran M
Senior
May 16, 2018 3:05 PM UTC
Posted on May 16, 2018 at 17:05

Hi Imen,

0690X0000060KkvQAE.png

When  i clear pinouts and select LPUART it will go to GPIOC instead of GPIOG.

Thanks

Phanirajkiran

Tesla DeLorean
Guru
May 16, 2018 5:12 PM UTC
Posted on May 16, 2018 at 17:12

V4.24.0 is NOT current, try using the current version to confirm if the issue exists or has been fixed in the intervening months...

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Nawres GHARBI
Nawres GHARBIBest answer
ST Technical Moderator
May 21, 2018 9:10 AM UTC
Posted on May 21, 2018 at 11:10

Hi 

Phanirajkiran, 

When loading the board, please select init peripherals and the LPUART will be at the right port. 

Enabling manually the peripheral will select the first available port and not the dedicated one on the board