Skip to main content
Herm
Associate II
Jan 23, 2020 10:44 AM UTC
Solved

BUG: CubeMX/CubeIDE ignores changes in initialization order.

Using Project Manager -> Advanced Settings -> Generated Function Calls you can change the initialization order. However this setting is ignored when writing the code.

You have to manually change the order in the .ioc file in this line:

ProjectManager.functionlistsort=1-MX_GPIO_Init-GPIO-false-HAL-true,2-SystemClock_Config-RCC-false-HAL-false,3-MX_DMA_Init-DMA-false-LL-true,4-MX_LPUART1_UART_Init-LPUART1-false-LL-true,5-MX_TIM20_Init-TIM20-false-LL-true,6-MX_USART3_UART_Init-USART3-false-HAL-true,7-MX_ADC1_Init-ADC1-false-LL-true,8-MX_ADC2_Init-ADC2-false-LL-true,9-MX_ADC3_Init-ADC3-false-LL-true,10-MX_ADC4_Init-ADC4-false-LL-true,11-MX_ADC5_Init-ADC5-false-HAL-true

Changing the numbers is what CubeMX is doing, but that is not enough. You have to actually reorder the items.

CubeIDE:

Version: 1.2.1

Build: 5190_20200115_1224 (UTC)

STM32CubeG4 Firmware Package V1.1.0 / 28-June-2019

This topic has been closed for replies.
Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
Jan 24, 2020 12:20 PM UTC

This was reported in another thread and I wrote a ticket about it at that time. It will be fixed in an upcoming release.

2 replies

Markus GIRDLAND
Markus GIRDLANDBest answer
ST Employee
Jan 24, 2020 12:20 PM UTC

This was reported in another thread and I wrote a ticket about it at that time. It will be fixed in an upcoming release.

CGala.1
Visitor II
Jul 21, 2021 9:33 PM UTC

@Markus GIRDLAND​ 

For what it's worth, this is still happening to me as of today using STM32CubeIDE 1.7.0 with a STM32F030C8T.

Spent hours trying to figure out what I had done wrong.