BUG: CubeMX/CubeIDE does not initialize TIM20.TRGO2 on STM32G474.
The configuration for the Timer 20 TRGO2 setting is not included in the generated source code. I verified using "git diff" that when changing the setting the only modified file is the .ioc.
I'm using the low level library for this timer. I haven't verifed if it happens with HAL as well.
CubeIDE:
Version: 1.2.1
Build: 5190_20200115_1224 (UTC)
STM32CubeG4 Firmware Package V1.1.0 / 28-June-2019