Skip to main content
PDiet.5
Associate
Mar 19, 2021 11:37 AM UTC
Solved

BSP_QSPI_Read on STM32H757I-EVAL from MT25TL01G misses first 6 bytes

I'm trying to do a simple read/write on the MT25TL01G flash that's present on the STM32H757I-EVAL evaluation board. However, when I'm using BSP_QSPI_Read, I'm missing the first 6 bytes of data. Reading via memory mapped mode works as expected.

Here's my initialization code. The QSPI clock should be running at 200MHz, according to CubeMX.

 /* QUADSPI parameter configuration*/
 hqspi.Instance = QUADSPI;
 hqspi.Init.ClockPrescaler = 3;
 hqspi.Init.FifoThreshold = 1;
 hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
 hqspi.Init.FlashSize = 26;
 hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
 hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
 hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
 if (HAL_QSPI_Init(&hqspi) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN QUADSPI_Init 2 */
 
 BSP_QSPI_DeInit(0);
 
 BSP_QSPI_Init_t init ;
 init.InterfaceMode = MT25TL01G_QPI_MODE;
 init.TransferRate = MT25TL01G_DTR_TRANSFER;
 init.DualFlashMode = MT25TL01G_DUALFLASH_ENABLE;
 
 if(BSP_QSPI_Init(0,&init) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 if(BSP_QSPI_EnableMemoryMappedMode(0) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 HAL_NVIC_DisableIRQ(QUADSPI_IRQn);
 /* USER CODE END QUADSPI_Init 2 */

Here's my code for read/write:

uint32_t address = 0;
char * writeData = "123456Hello world!";
char data[50] = {};
size_t size = strlen(writeData);
 
char qspi_data[50] = {};
memcpy(qspi_data, (void*)(QSPI_BASE_ADDRESS + address), size);
printf("Read via MemMap: %s\r\n", qspi_data); // works as expected (if it has been written already)
 
// Disable MemoryMappedMode
BSP_QSPI_DisableMemoryMappedMode(0);
 
// Erase sector
BSP_QSPI_EraseBlock(0, address, BSP_QSPI_ERASE_8K);
 
// Write data
BSP_QSPI_Write(0, (uint8_t*)writeData, address, size);
 
// Read data
BSP_QSPI_Read(0, (uint8_t*)data, address, size)
 
printf("Read %s from QSPI\r\n", data); // prints: "Hello world!" instead of "123456Hello world!"

All the BSP_QSPI_* function calls return without error.

What am I doing wrong?

This topic has been closed for replies.
PDiet.5
PDiet.5Best answer
Associate
May 20, 2021 9:12 AM UTC

By changing the dummy cycles I did manage to fix this, but it caused the QSPI / flash to lock up when changing to and from memory mapped mode and other troubles.

I believe that the problem was caused by BSP_QSPI_DisableMemoryMappedMode/BSP_QSPI_EnableMemoryMappedMode not working as expected?

Instead, I used the following code to change from memory mapped mode to indirect mode and vice versa by resetting the HAL and the MT25TL01G each time.

Memory mapped to indirect:

extern QSPI_HandleTypeDef hqspi;
 
 HAL_QSPI_DeInit(&hqspi);
 hqspi.Instance = QUADSPI;
 hqspi.Init.ClockPrescaler = 3;
 hqspi.Init.FifoThreshold = 1;
 hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
 hqspi.Init.FlashSize = 26;
 hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
 hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
 hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
 if (HAL_QSPI_Init(&hqspi) != HAL_OK)
 {
 Error_Handler();
 }
 
 if (BSP_QSPI_DisableMemoryMappedMode(0) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 
 BSP_QSPI_DeInit(0);
 
 BSP_QSPI_Init_t init;
 init.InterfaceMode = MT25TL01G_QPI_MODE;
 init.TransferRate = MT25TL01G_DTR_TRANSFER;
 init.DualFlashMode = MT25TL01G_DUALFLASH_ENABLE;
 
 extern BSP_QSPI_Ctx_t QSPI_Ctx[QSPI_INSTANCES_NUMBER];
 QSPI_Ctx[0].IsInitialized = QSPI_ACCESS_NONE;
 
 if (BSP_QSPI_Init(0, &init) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }

Indirect to memory mapped:

extern QSPI_HandleTypeDef hqspi;
 
 HAL_QSPI_DeInit(&hqspi);
 hqspi.Instance = QUADSPI;
 hqspi.Init.ClockPrescaler = 3;
 hqspi.Init.FifoThreshold = 1;
 hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
 hqspi.Init.FlashSize = 26;
 hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
 hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
 hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
 if (HAL_QSPI_Init(&hqspi) != HAL_OK)
 {
 Error_Handler();
 }
 
 BSP_QSPI_DeInit(0);
 
 BSP_QSPI_Init_t init;
 init.InterfaceMode = MT25TL01G_QPI_MODE;
 init.TransferRate = MT25TL01G_DTR_TRANSFER;
 init.DualFlashMode = MT25TL01G_DUALFLASH_ENABLE;
 
 extern BSP_QSPI_Ctx_t QSPI_Ctx[QSPI_INSTANCES_NUMBER];
 QSPI_Ctx[0].IsInitialized = QSPI_ACCESS_NONE;
 
 if (BSP_QSPI_Init(0, &init) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 if (BSP_QSPI_EnableMemoryMappedMode(0) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 HAL_NVIC_DisableIRQ(QUADSPI_IRQn);

The key point was to set

extern BSP_QSPI_Ctx_t QSPI_Ctx[QSPI_INSTANCES_NUMBER];
 QSPI_Ctx[0].IsInitialized = QSPI_ACCESS_NONE;

before calling BSP_QSPI_Init(), to get the BSP driver to properly re-initialize the MT25TL01G driver.

I realize this is probably not the most efficient or elegant solution, but I did not have any more time to dig any deeper and was just happy I got it working somehow.

5 replies

Tesla DeLorean
Guru
Mar 19, 2021 4:55 PM UTC

Too many dummy cycles, wrong address width/size setting? ie mismatch in understanding of SW/HW on STM32 side and QSPI device

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
PDiet.5
PDiet.5AuthorBest answer
Associate
May 20, 2021 9:12 AM UTC

By changing the dummy cycles I did manage to fix this, but it caused the QSPI / flash to lock up when changing to and from memory mapped mode and other troubles.

I believe that the problem was caused by BSP_QSPI_DisableMemoryMappedMode/BSP_QSPI_EnableMemoryMappedMode not working as expected?

Instead, I used the following code to change from memory mapped mode to indirect mode and vice versa by resetting the HAL and the MT25TL01G each time.

Memory mapped to indirect:

extern QSPI_HandleTypeDef hqspi;
 
 HAL_QSPI_DeInit(&hqspi);
 hqspi.Instance = QUADSPI;
 hqspi.Init.ClockPrescaler = 3;
 hqspi.Init.FifoThreshold = 1;
 hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
 hqspi.Init.FlashSize = 26;
 hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
 hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
 hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
 if (HAL_QSPI_Init(&hqspi) != HAL_OK)
 {
 Error_Handler();
 }
 
 if (BSP_QSPI_DisableMemoryMappedMode(0) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 
 BSP_QSPI_DeInit(0);
 
 BSP_QSPI_Init_t init;
 init.InterfaceMode = MT25TL01G_QPI_MODE;
 init.TransferRate = MT25TL01G_DTR_TRANSFER;
 init.DualFlashMode = MT25TL01G_DUALFLASH_ENABLE;
 
 extern BSP_QSPI_Ctx_t QSPI_Ctx[QSPI_INSTANCES_NUMBER];
 QSPI_Ctx[0].IsInitialized = QSPI_ACCESS_NONE;
 
 if (BSP_QSPI_Init(0, &init) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }

Indirect to memory mapped:

extern QSPI_HandleTypeDef hqspi;
 
 HAL_QSPI_DeInit(&hqspi);
 hqspi.Instance = QUADSPI;
 hqspi.Init.ClockPrescaler = 3;
 hqspi.Init.FifoThreshold = 1;
 hqspi.Init.SampleShifting = QSPI_SAMPLE_SHIFTING_NONE;
 hqspi.Init.FlashSize = 26;
 hqspi.Init.ChipSelectHighTime = QSPI_CS_HIGH_TIME_4_CYCLE;
 hqspi.Init.ClockMode = QSPI_CLOCK_MODE_0;
 hqspi.Init.DualFlash = QSPI_DUALFLASH_ENABLE;
 if (HAL_QSPI_Init(&hqspi) != HAL_OK)
 {
 Error_Handler();
 }
 
 BSP_QSPI_DeInit(0);
 
 BSP_QSPI_Init_t init;
 init.InterfaceMode = MT25TL01G_QPI_MODE;
 init.TransferRate = MT25TL01G_DTR_TRANSFER;
 init.DualFlashMode = MT25TL01G_DUALFLASH_ENABLE;
 
 extern BSP_QSPI_Ctx_t QSPI_Ctx[QSPI_INSTANCES_NUMBER];
 QSPI_Ctx[0].IsInitialized = QSPI_ACCESS_NONE;
 
 if (BSP_QSPI_Init(0, &init) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 if (BSP_QSPI_EnableMemoryMappedMode(0) != BSP_ERROR_NONE)
 {
 Error_Handler();
 }
 HAL_NVIC_DisableIRQ(QUADSPI_IRQn);

The key point was to set

extern BSP_QSPI_Ctx_t QSPI_Ctx[QSPI_INSTANCES_NUMBER];
 QSPI_Ctx[0].IsInitialized = QSPI_ACCESS_NONE;

before calling BSP_QSPI_Init(), to get the BSP driver to properly re-initialize the MT25TL01G driver.

I realize this is probably not the most efficient or elegant solution, but I did not have any more time to dig any deeper and was just happy I got it working somehow.

Roberto C
Associate II
Oct 28, 2021 12:15 PM UTC

Hi PDiet.5 

I'm having same troubles.

Could you better explain how and where you changed the dummy cycles to solve the missing 6 bytes?

What value you used to solve it?.

Thnx in advance

Roberto.

Tesla DeLorean
Guru
Oct 28, 2021 12:40 PM UTC

The data sheet should detail the frequency vs dummy cycles to allow the memory to do an initial fetch into its page buffer.

​

I​t has a 0 to 15 range programmed into a register on the memory side, and then specified on the READ command instance.

​

Usually there's a Set/Program Dummy Cycles in the initialization code, so both memory and MCU have a consistent expectation.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Roberto C
Associate II
Oct 28, 2021 1:10 PM UTC

Thnx for infos!

..but before to change it I tried to implement the above functions ("Memory mapped to indirect" and "indirect to Memory mapped") and it seems to solve also the original trouble in this question ("missing first 6 bytes")..

Still investigating over it....