Skip to main content
Graduate
January 15, 2026
Question

[BLE] CubeMX does not generate read characteristic update function in "custom_app.c"

Hi,

I'm building a BLE application using custom template in STM32CubeMX. I have two services. The first one has only one characteristic with the properties "Read" and "Write without response". The second service has two characteristics, both with "Read" and "Notify" properties.

The code generated in "custom_app.c" have the function:

void Custom_<Srv2Char1>_Update_Char(void){...}
void Custom_<Srv2Char1>_Send_Notification(void){...}
void Custom_<Srv2Char2>_Update_Char(void){...}
void Custom_<Srv2Char2>_Send_Notification(void){...}

However, no function is generated for the characteristic of the first service. I expected to have a function like this:

void Custom_<Srv1Char1>_Update_Char(void){...}

 

I performed some tests:

  1. Used shorter names for the characteristics.
  2. Created two new characteristics, one in service 1 and the other in service 2, both with only the "Read" property enabled.

In both cases, no "Update_Char" function was generated.


I don’t know if this behavior is correct. If it is, how am I supposed to respond to a "Read" request?
Here’s what I’m doing:

void Custom_STM_App_Notification(Custom_STM_App_Notification_evt_t *pNotification)
{
 switch (pNotification->Custom_Evt_Opcode)
 {
 ...
 ...
 case CUSTOM_STM_<Srv1Char1>_READ_EVT:
	 ...
 Custom_STM_App_Update_Char(CUSTOM_STM_<Srv1Char1>, (uint8_t*) UpdateCharData);
	 ... 
 break;
 ...
 ...
 }
 return;
}

 

Some other info:

  • STM32CubeMX version 6.16.1
  • STM32IDE version: 2.0.0
  • The ".ioc" file is attached 

 

Thanks!

1 reply

Ghofrane GSOURI
ST Technical Moderator
January 16, 2026

Hello @DecaMeron 

Your contribution is greatly appreciated.

A ticket has been escalated to dev team under the internal ticket number  225400 and it will be fixed as soon as possible.

I will keep you posted with updates.

 

THX

Ghofrane

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.