Skip to main content
Martin294
Associate III
January 28, 2021
Question

Backup registers are cleared on reset - STM32G474

Hi all,

I have a STM32G474 and data in backup registers (eg. LL_RTC_BKP_DR0) are cleared after reset or power cycle (3.3 V battery is present!).

Code is generated by CubeMX with LL drivers. I enabled RTC and disabled all tampers.

In the main code, I can write to the registers (and readback or check via debugger/SFR view).

However, if I restart the debugger, press the reset button (with or without debugger connected) or switch of VCC (with VBAT present from a CR2032 battery), backup registers are all 0.

As I understand it, this could be caused by a RTC domain reset or a tamper event. I have neither, as far as I can tell. What could be wrong? Is there an example for this?

Regards, Martin

This topic has been closed for replies.

5 replies

waclawek.jan
Super User
January 28, 2021

> As I understand it, this could be caused by a RTC domain reset [....] I have neither,

But you've said:

> Code is generated by CubeMX with LL drivers.

So, isn't there a RTC domain reset in the generated code?

In debugger, try to place a data breakpoint on the respective register in RCC through which the RTC domain is reset.

JW

Martin294
Martin294Author
Associate III
January 28, 2021

Nice idea... tried to put an SWV trace on the BKP_DR0 register (0x40002500), but this does not work. Setting a data trace comparator to an SRAM variable works though.

However, you have a good point. I stepped through the init and the generated SystemClock_config contains

 LL_PWR_EnableBkUpAccess();

 LL_RCC_ForceBackupDomainReset();

 LL_RCC_ReleaseBackupDomainReset();

So here is the backup domain reset as you suspected.

Why would they do this? It's the whole point of the backup domain of preserving data... How can I turn this off? I have not found a setting for this in the code generator.

Of course I can delete the reset from the generated code, but each time I regenerate it via CubeMX, this gets overwritten.

Thanks! Martin

Martin294
Martin294Author
Associate III
January 28, 2021

It seems I am not the only one falling into this trap:

https://community.st.com/s/question/0D50X00009XkX3P/bug-rtc-cannot-be-used-when-code-for-rcc-is-generated-using-ll?t=1587464385508

A google search on "LL_RCC_ForceBackupDomainReset" finds other occurences.

It seems this is a CubeMX bug? Should I report this (where)?

Khouloud OTHMAN
Associate
January 29, 2021

Hi @Community member​ ,

This issue has been already detected and reported internally for fix. I'll keep you posted with the updates.

Sorry for the inconvenience.

Linked here the same problem with a workaround preposition. It may work for you.

Thanks for you patience.

Khouloud.

Martin294
Martin294Author
Associate III
January 30, 2021

Thanks for the clarification! Let's hope this is fixed soon.

- Martin