Skip to main content
Associate II
October 9, 2025
Solved

B-WL5M-SUBG1 Sigfox_AT_Slave Application LPUART has wrong pin configurations

As you can see below picture, B-WL5M-SUBG1 Connectivity Expansion Board's UART pins are PC0 and PC1:

MonaRoza_1-1760020919303.png

But in the STM32Cube_FW_WL_V1.3.1 repository Sigfox_AT_Slave application for B-WL5M-SUBG1 describes uart pins are PA3 and PA2:

MonaRoza_0-1760020898896.png

So in this case, application's UART AT interface doesn't work. Buf if you change LPUART1 pin configurations, it works fine: 

MonaRoza_2-1760021099296.png

 

Thank you for your interest.

This topic has been closed for replies.
Issamos
IssamosBest answer
Super User
October 9, 2025

Hello @Mona-Roza 

As you can see on the Readme file of the example:

« Connect the Connectivity Expansion Board to your PC with an external STLINK-V3SET. »

and the STLINK-V3SET is usually connected to the board throw the STDC14 connector (CN3). According to the table 14 of the UM3127: the LPUART is connected to PA2 and PA3: 

Issamos_0-1760035991266.png

so, the example works fine as it is if you are using the CN3. If you want to use the CN1, you should change the LPUART pins to PC0 and PC1 but this is not the official implementation. 

Best Regards.

II

 

3 replies

ST Technical Moderator
October 9, 2025

Hello @Mona-Roza ,

 

Let me thank you for your feedback.

Your request is under investigation, and I will get back to you ASAP.

 

Thanks.

Mahmoud

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Issamos
IssamosBest answer
Super User
October 9, 2025

Hello @Mona-Roza 

As you can see on the Readme file of the example:

« Connect the Connectivity Expansion Board to your PC with an external STLINK-V3SET. »

and the STLINK-V3SET is usually connected to the board throw the STDC14 connector (CN3). According to the table 14 of the UM3127: the LPUART is connected to PA2 and PA3: 

Issamos_0-1760035991266.png

so, the example works fine as it is if you are using the CN3. If you want to use the CN1, you should change the LPUART pins to PC0 and PC1 but this is not the official implementation. 

Best Regards.

II

 

Mona-RozaAuthor
Associate II
October 10, 2025

Hello,

I'm new in ST world, sorry for my missunderstood. In my case I'm trying to use double-MCU setup in my custom. So I didn't thought this kind of examples just for PC. 

Thank you for your interest.
Best regards, 
Mona-Roza