Skip to main content
CLiu.0
Visitor II
Feb 11, 2020 1:34 PM UTC
Question

B-L475-IOT01A+FREERTOS+X-CUBE-BLE1 does not build

Hi there,

I am using the latest CubeMX to generate code for B-L475-IOT01A with FREERTOS and X-CUBE-BLE1 4.4.0. However the code it generate does not even build. I tried various samples, including SensorDemoBLESensor, Beacon, but yield the same result.

The build message indicated that MX_BlueNRG_MS_Init() is missing. Apparently it is missing an entire suite of source code. I attempt to port the code over from a Nucleo sample code but was unsuccessful.

Please kindly help to fix. Thanks!

This topic has been closed for replies.

2 replies

Karl Yamashita
Principal
Feb 11, 2020 5:02 PM UTC

Yeah I've complained about the same issue over a year ago with support. I too can't get it to compile without so many errors. I still haven't seen ST fix the compile errors since then.

If a reply has proven helpful, click on Accept as Solution so that it'll show at top of the post.CAN Jammer an open source CAN bus hacking toolCANableV3 Open Source
DGarc.5
Associate
Mar 22, 2023 2:24 PM UTC

Any answer?