Skip to main content
Explorer
July 24, 2025
Question

Avoiding CubeMX to remove user changes to original code

  • July 24, 2025
  • 1 reply
  • 209 views

Hi

I'm working on a firmware based on a STM32WL libraries example, specifically LoraWan_End_Node for WL55JC.

The example sends data every 10s but also performs several operations using leds and timer. I need to remove some parts of this original code and sometimes write outside the USER_CODE_BEGIN/END sections.

The problem is, when I use CubeMX it will restore the original code where I changed it. Is there any way to prevent this restoring? And at the same time be able to use the CubeMX.

Thanks 

This topic has been closed for replies.

1 reply

Andrew Neil
Super User
July 24, 2025

@smassardi wrote:

Is there any way to prevent this restoring?


No. That is the defined behaviour - only code within the USER CODE markers is retained.

You will have to manually merge your changes back into the code.

There is an option to have CubeMX backup the files that it re-generates:

AndrewNeil_0-1753354022006.png

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.