Skip to main content
eBirdman
Senior
Feb 8, 2021 7:53 PM UTC
Question

Are STM32F7Cube code examples configured with CubeMX ?

Hi, The SDK package provided in STM32F7Cube has many code examples on all topics but is that code initialized with CubeMX ? Or, otherwise , if it is not , in order to reconfigure or customize it the user has to manually merge that code with the one generated by STM32CubdeMX ? I know that in the past STM Cube packages were provided with pre-CubeMX old examples. What is the current situation?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Feb 8, 2021 8:11 PM UTC

I think it's a bit hit-and-miss, they either have an IOC file or they don't

Personally I prefer examples that aren't choked full of crap, and actually written by an engineer who knew what they were doing / wanted to achieve.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
eBirdman
eBirdmanAuthor
Senior
Feb 8, 2021 8:34 PM UTC

CubeMX is designed exactly for that : to (re)configure the project to whatever the developer needs. I've been away from STM for last 2 years but remember back then working with STM32F4 every example code I had to change manually to merge with my own generated CubeMX configuration... CubeMX was like "you-can-use-it-too" unrelated to the examples... So I wonder may be STM has advanced enough to provide CubeMX generated examples for their most advanced MCUs which definitely need GUI kind of configurator ?