Skip to main content
GreenGuy
Senior III
March 10, 2023
Question

Anybody else seen when in CubeMX selecting Enable SD register Callbacks also causes SDRAM register callbacks to automatically flip to enable when saving and generating code?

STM32CubeIDEVersion: 1.12.0

STM32CubeMX: Version: 6.8.0-RC4

I think this is a BUG!

When in CubeMX perspective in CubeIDE, in the project manager Advanced tab, in the Register Callback window, if you ENABLE the register callback for SD and save or generate code, the SDRAM register callback setting automatically flips to ENABLE. The two setting should be mutually exclusive and if you are not using SDRAM in your code this may cause numerous compile errors. The ENABLE setting for SDRAM does not change when you initially select ENABLE for SD (SD card), but only after you click on save or generate. Kind of sneaky and if you blink you will miss it.

This topic has been closed for replies.

4 replies

GreenGuy
GreenGuyAuthor
Senior III
March 10, 2023

The versions posted up front in the question are the latest versions for the Linux version. And yes I will be putting in a ticket on it.

Piranha
Principal III
March 11, 2023

Time to stop playing with kids cubes and moving to adult software development. ;)

GreenGuy
GreenGuyAuthor
Senior III
March 13, 2023

Development has reproduced the error in the latest version and previous versions so they are aware.

GreenGuy
GreenGuyAuthor
Senior III
March 13, 2023

Piranha, what do you consider adult software?