Skip to main content
vmekr
Associate
Jan 10, 2019 10:05 AM UTC
Solved

Any difference between STM32CUBE_MX And Atollic_TrueStudio?

Right at the moment I have 2 software, Atollic TrueStudio & STM32CUBE_MX . I am pretty confused, which one to use for an STM32-Cortex M4 ?

Is there any difference between Atollic TrueStudio & STM32CUBE_MX software?

Which one is stable?

thanks

This topic has been closed for replies.
After Forever
After ForeverBest answer
Senior III
Jan 10, 2019 11:05 AM UTC

They are two completely different things. Lemons and apples.

STM32CubeMX is a tool to generate the initialization code and the skeleton of the project in one of the supported IDE formats.

Atollic TrueStudio is an IDE with an integrated compiler (GNU GCC) and debugger (GNU GDB).

Use the former tool for initial code generation (and later re-generation), use the latter tool for actual development.

3 replies

After Forever
After ForeverBest answer
Senior III
Jan 10, 2019 11:05 AM UTC

They are two completely different things. Lemons and apples.

STM32CubeMX is a tool to generate the initialization code and the skeleton of the project in one of the supported IDE formats.

Atollic TrueStudio is an IDE with an integrated compiler (GNU GCC) and debugger (GNU GDB).

Use the former tool for initial code generation (and later re-generation), use the latter tool for actual development.

vmekr
vmekrAuthor
Associate
Jan 10, 2019 11:22 AM UTC

Thanks @After Forever​ .

If I understand correctly, Pin & Clock can be configured and code generated in STM32CubeMX which is an integrated-Perspective in the Atollic_TrueStudio. Then the another perspective in Atollic (C/C++ ) can be used for the further development and debugging. Am I right?

After Forever
Senior III
Jan 10, 2019 11:26 AM UTC

Yes, that's right. I use STM32CubeMX as a stand-alone tool (not as an Eclipse plugin in Atollic), but I guess it's the same thing.