Skip to main content
AR L
Associate
Jul 1, 2019 9:44 AM UTC
Question

About configuring the pins.

We are using STM32F207ZG and while configuring it with the help of STM32IDE we are facing some conflicts like we have used USART1(Asynchronous mode with only Rx and Tx) . It is showing conflict if we use USART1_CTS and USART1_RTS pins as GPIO pins. The error showing is "Partly disabled conflict with use of GPIO pin". My doubt is that can we use them as GPIO if conflict is there or else its reserved.

This topic has been closed for replies.

2 replies

RAlex
Visitor II
Jul 1, 2019 10:54 AM UTC

Where is the error stated?

If i configure the usart1 as asynchronous and Hardware flow control is disabled there is no error showing up.

If you configure the Pins PA11&&PA12 to GPIOs usb_otg_fs will not work.

Do you need USB?

Can you post the error or a picture from your Pinout overview?

AR L
AR LAuthor
Associate
Jul 1, 2019 12:37 PM UTC

Thank you for your response.

Unfortunately I am not able to capture the error. I am not using it for USB_OTG_FS I am using it as GPIO.