Skip to main content
TNaxi
Associate II
Nov 27, 2019 1:40 AM UTC
Question

A lot of errors in STM32Cube_FW_F0_V1.11.0

Error 1:

MX version: STM32CubeMX 5.4.0

Firmware: STM32Cube_FW_F0_V1.11.0

Compiler: IAR

MCU: Any in F0 series

Compiling error:

Error[Pe147]: declaration is incompatible with "__interwork __softfp void assert_failed(uint8_t *, uint32_t)" (declared at line 308 of "… main.c�?

Analysis:

The function, assert_failed(), generated by STM32CubeMX in main.c is defined as follows:

void assert_failed(char *file, uint32_t line) {}

The protoypte of this function should be below as mentioned in Release notes:

void assert_failed(uint8_t *file, uint32_t line) {}

Error 2:

MX version: STM32CubeMX 5.4.0

Firmware: STM32Cube_FW_F0_V1.11.0

Compiler: IAR

MCU: STM32F042

Compiling error:

Error[Pe136]: “… stm32f0xx_hal_crc.h has no field "DefaultPolynomialUse�? “

Analysis:

On the one hand, the generating Polynomial in CRC peripheral of STM32F042 is not programmable, the macro CRC_POL_POL is undefined, as a result, DefaultPolynomialUse is not a member of struct CRC_InitTypeDef.

On the other hand, the code generated by STM342CubeMX has the statement with DefaultPolynomialUse as follows:

hcrc.Init.DefaultPolynomialUse = DEFAULT_POLYNOMIAL_ENABLE;

Error 3:

MX version: STM32CubeMX 5.4.0

Firmware: STM32Cube_FW_F0_V1.11.0

Compiler: IAR

MCU: STM32F072

Linker error:

Error[Li005]: no definition for "HAL_CRCEx_Init" [referenced from … crc.o]

Analysis:

The code in function MX_CRC_Init() generated by STM32CubMX has the statements below:

if (HAL_CRCEx_Init(&hcrc) != HAL_OK) …

As mentioned in Release notes, HAL_CRCEx_Init has been abandoned and undefined and should not be used.

Recommendations on STM32CubeMX:

R1: A specific channel or mailbox should be created or provided to make developers submitting bug report conveniently.

R2: The path where the STMCubMX Repository should be configurable by developers.

This topic has been closed for replies.

11 replies

Khouloud ZEMMELI
ST Employee
Nov 27, 2019 7:19 AM UTC

​hello @TNaxi​ ,

Could you please share your iocs files for each error ?

Thanks,

Khouloud.

Khouloud ZEMMELI
ST Employee
Nov 27, 2019 8:13 AM UTC

@TNaxi​ : Only error 2 is reproduced -> it will be fixed.

need your ioc file for error 1 and for error 3.

Thanks and Best Regards,

Khouloud

​

TNaxi
TNaxiAuthor
Associate II
Nov 28, 2019 1:53 AM UTC
Dear Khouloud Zemmeli,
The attachment is the ioc file we used.
Thanks and Best Regards,
Tian Naxin
Pavel A.
Nov 28, 2019 2:53 AM UTC

> R2: The path where the STMCubMX Repository should be configurable by developers.

The path is already configurable.

What you probably want is to have two separate independent repository paths: A. for CubeMX itself to install & update its templates(?) etc. and B. the path to use in generated projects when user chooses to create references vs. copy files.

Like it was in older Cube versions.

-- pa

Abhishek Deouskar
Associate III
Nov 28, 2019 9:06 AM UTC

I am facing issues in the CAN section of the STM32Cube_FW_F0_V1.11.0.

My .ioc file is attached for your reference.

The HAL_CAN_AddTxMsg(..args..) goes to Hardfault Handler at the line:

 /* Store the Tx mailbox */
 *pTxMailbox = (uint32_t)1 << transmitmailbox;

I wrote a simple snippet for CAN Transmit as:

void TransmitCAN(uint32_t StdID, uint8_t *data_arr, uint8_t DLC)
{
	CAN_TxHeaderTypeDef	TxMsg = {0};
 
	TxMsg.StdId = StdID;
	TxMsg.IDE = CAN_ID_STD;
	TxMsg.RTR = CAN_RTR_DATA;
	TxMsg.DLC = DLC;
	TxMsg.TransmitGlobalTime = DISABLE;
 
	HAL_CAN_AddTxMessage(&hcan, &TxMsg, data_arr, (uint32_t*)CAN_TX_MAILBOX0);
 
	if((hcan.Instance->TSR & CAN_TSR_TXOK0) != RESET)
	{
		if((hcan.Instance->TSR & CAN_TSR_TXOK1) != RESET)
		{
			if((hcan.Instance->TSR & CAN_TSR_TXOK2) != RESET)
			{
				Error_Handler();
			}
		}
	}
}

I called the same in a while(1) loop in main.c…

The same code works for F4 or F3 series controllers. Also the code I had written for CAN using the V1.9 for the same board works. So I have eliminated Hardware issues at my end.