Skip to main content
ADing.1
Associate II
Oct 24, 2023 2:06 PM UTC
Question

X-NUCLEO-LPM01A and STM32 Cube Monitor-Power: Cannot detect board on Debian 12 Linux

I have installed STM32 Cube Monitor Power on Debian 12 (64 bit) and have connected a LPM01A via USB. When I run the power monitor, no board shows up in the drop down menu. I have tried the two versions of the power monitor available on the ST website.

Running lsusb, I can see a device called `STMicroelectronics Virtual COM Port`, which corresponds to the LPM01A.

How can I get the power monitor to connect to the LPM01A?

This topic has been closed for replies.

1 reply

PDEFO.1
ST Employee
Dec 4, 2023 9:14 AM UTC

Hello,

As indicated in User Manual UM2202 (chapter 2.1), supported operating systems include Linux, but only distributions Red Hat, Fedora, and Ubuntu, has been tested.

We recommand to use these distributions.

Regards