Skip to main content
Jono Makepeace
Associate
Feb 4, 2021 9:28 AM UTC
Question

What is STM32CubeMonitor error: PayloadTooLargeError: request entity too large ?

Hi, I am getting the following error when trying to deploy:

PayloadTooLargeError: request entity too large

  at readStream (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\raw-body\index.js:155:17)

  at getRawBody (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\raw-body\index.js:108:12)

  at read (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\body-parser\lib\read.js:77:3)

  at jsonParser (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\body-parser\lib\types\json.js:135:5)

  at Layer.handle [as handle_request] (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\express\lib\router\layer.js:95:5)

  at trim_prefix (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\express\lib\router\index.js:317:13)

  at C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\express\lib\router\index.js:284:7

  at Function.process_params (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\express\lib\router\index.js:335:12)

  at next (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\express\lib\router\index.js:275:10)

  at cors (C:\Users\JonoM.AFRICA\AppData\Local\STM32CubeMonitor\resources\app.asar\node_modules\cors\lib\index.js:188:7)

I am using the Basic_Flow example, selecting 3 u32 variables. I used an .axf file generated in uVision to pull the symbols into STM32CubeMonitor.

This topic has been closed for replies.

4 replies

Richard.Chvr
ST Technical Moderator
Apr 14, 2022 9:59 AM UTC

hello @Jono Makepeace​ 

can you share your axf file

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
YLee.10
Visitor II
Aug 30, 2022 1:57 AM UTC

Hi, I get a similar error when trying to deploy.

0693W00000Su1zsQAB.jpgI noticed this happens when I try to select multiple elements of an array. Single variables do not result in this error.

I am trying to display an array in a real-time graph, and have previously succeeded following the advice from the how-to-watch-an-array-using-stm32cubemonitor question on this forum.

However, after changing to a different STMCUBEIDE project, I could no longer deploy after selecting more than 1 element of the array. The workspace also crashes after the error occurs, even if previously working flows are deployed. Only restarting the monitor can revert the work space to a previous functioning state to deploy other functioning flows.

Any help on shedding light on this matter would be greatly appreciated. Thank you!

JPerr.2
Associate II
Sep 15, 2022 8:07 AM UTC

I get the same issue. It might also be related to reading array elements. When it happens, I have many troubles to get rid of the error. It would be great to know what's the initial condition triggering the error and to get properly out of this error state.

pdematteis
Associate
Oct 2, 2024 10:46 AM UTC

It is possible to edit the settings file in the user folder like this:

C:\Users\<userame>\.STMicroelectronics\stm32cubemonitor\settings.js

 /** The maximum size of HTTP request that will be accepted by the runtime api.
 * Default: 5mb
 */
 //apiMaxLength: '5mb',
 apiMaxLength: '10mb',