Skip to main content
Associate
May 22, 2025 9:15 AM UTC
Question

ULPMark™-CoreMark score

We were following the ULPMark™-CoreMark User Guide for getting the ulp mark score but the STM X-NUCLEO-LPM01A is always throwing up some error and the LD2(ErrorLED) turns on causing issues. Also if in the case it runs its always telling    “>! Validation failed, too little runtime: 0.014000000000000234” “>! Set iterations above 749999 for Energy run”. Even after using the same parameters its throwing the same error. Also at 1ms the connection is never achieved and fails.

It would be great if you can guide us on this.

    This topic has been closed for replies.

    6 replies

    Andrew Neil
    Super User
    May 22, 2025 9:19 AM UTC

    Welcome to the forum.

    Please see How to write your question to maximize your chances to find a solution for best results.

     


    @Abhilasha wrote:

    throwing up some error .


    What error, exactly?

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    AbhilashaAuthor
    Associate
    May 22, 2025 9:27 AM UTC

    so i have been following the guide and in the iotconnect for ulpmark-cm, the errors are being shown on the console as below :
    000196.568: Checking results for run 2: Energy
    000196.580: Validation: Getting self-reported frequency
    000196.591: Validation: Getting session iterations
    000196.603: Validation: Run mode
    000196.619: Validation: temperature
    000196.635: Validation: Compute frequency from ticks
    000196.650: Validation: EMON voltage (mV)
    000196.659: Validation: DUT Library Name
    000196.667: Validation: Library Compiler Name
    000196.676: Validation: Library Compiler Flags
    000196.689: Validation: Runtime >10s and iterations at least 10
    000196.701: >! Validation failed, too little runtime: 0.014000000000000234
    000196.713: ystem
    000196.722: Checking results for run 3: Energy (3V)

    Even if I set the iterations as required the same error is thrown with a bigger no for iterations.

    and even in between the running  the connection is lost (With red light LD2 on over nucleo-lpm01a board) and keeps skipping the runs telling "another script running already"

    Amel NASRI
    ST Technical Moderator
    May 22, 2025 10:31 AM UTC

    Hi @Abhilasha ,

    May I know the product for which you are looking for the ULPMark™-CoreMark score?

    -Amel

    To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.