STM32G0B1RE and SRC1M1 for Power Delivery charge not connecting to STM32Cubemonitor
- 5 replies
- 2129 views
Hello, I'm using a STM32G0B1RE and a nucleo SRC1M1 in order to charge and communicate with a tablet in power delivery mode with 5V 3A. I followed the following tutorial: STM32StepByStep:Getting started with USB-Power Delivery Source - stm32mcu (stmicroelectronics.cn) from STM, at first it kinda worked, I had a connection with the tablet in the traces with it confirming it does take 5V and 3A as well as the IN SOPs:002 H:0x0041 GOODCRC message but since it was connected on a hub, it kept turning on and off. So I took the cable for the ST off the hub and directly onto the computer (the nucleo is receiving 5V 3A from an external source) but since then when I go on the board selection and connect the tablet, it keeps disconnecting. I checked, there doesn't seem to be any loss of voltage, so I'm quite lost as to why the board doesn't want to connect with the app.
I also changed the STM32, changed computer, changed cable between the tablet and nucleo, nothing changes. I haven't been able to change the nucleo or the cable between the computer and the STM32 because I only have one each. I also made a new project, following the directions again and no changes. Furthermore, the tablet is charging, albeit not to 3A (1.406A).
I have attached a screenshot of the interface on port selection when the tablet is connected (not refreshed because otherwise it takes me back to the board selection with the message of "please connect a board")