Skip to main content
MKori.1
Associate III
Mar 10, 2023 10:14 AM UTC
Solved

STM32CubeMonitor - Trigger SW Reset

Hello,

I would like to trigger a STM32 device reset from inside STM32CubeMonitor.

I'm developing an application using STM32CubeIDE and STM32CubeMonitor. Duringe measuring of my variables via STM32CubeMonitor it is possible that my device gets into a reduced function safe state (on purpose). Then it would be very helpful to trigger a device reset via a button like I'm able to do during debugging in STM32CubeIDE.

I understand currently only the topics: Read, Start and Stop are available for a probe-node. Is it possible to trigger a reset via additional (maybe undocumented) options or is this feature planned in a future release?

If not is there a workaround available? I tried to connect to the GDB server opened by the probe-node after starting the acquisition but wasn't successful. As far as a saw it, the server is always opend on a different port?!.

Thank you

Best regards

Martin

This topic has been closed for replies.
Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Mar 30, 2023 7:37 AM UTC

Hello @MKori.1​ 

There's no such option in STM32CubeMonitor, as a workaround you may also try to use write node in order to write a variable to trigger an event in your application to reset.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

6 replies

MKori.1
MKori.1Author
Associate III
Mar 28, 2023 8:50 AM UTC

As a workaround I can trigger a reset via STM32ProgrammerCLI. But this doesn't work when the connection is active.

Richard.Chvr
Richard.ChvrBest answer
ST Technical Moderator
Mar 30, 2023 7:37 AM UTC

Hello @MKori.1​ 

There's no such option in STM32CubeMonitor, as a workaround you may also try to use write node in order to write a variable to trigger an event in your application to reset.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MKori.1
MKori.1Author
Associate III
Mar 30, 2023 9:18 AM UTC

Hello,

thank you for your idea, this should work for me. As the debugger interface in the background is already able to reset the device is it planned to update the probe-node? Is there a place to post such ideas? Something like "Issues" in Github.

Richard.Chvr
ST Technical Moderator
Mar 30, 2023 12:33 PM UTC

I will raise a Change request to the dev. team to post your proposal.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
MKori.1
MKori.1Author
Associate III
Nov 25, 2024 4:56 PM UTC

Hi @Richard.Chvr ,

is there any update on that proposal available?

Thank you!

Best regards

Richard.Chvr
ST Technical Moderator
Nov 27, 2024 1:34 PM UTC

Hi @MKori.1 ,

No update for the Sw reset implementation unfortunately, I try to push to get it in nest 1.10 release.

Regards

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.