Skip to main content
stephane.legargeant
ST Employee
Nov 19, 2020 5:20 PM UTC
Solved

STM32CubeMonitor-RF V2.6.0 released

New version 2.6.0 is released.

New features :

Some 802.15.4 RF tests are added to make certification tests easier :

  • In the transmitter test,it is possible to send MAC frames . The frame can be defined by the user.
  • In the receiver test, the LQI, ED, and CCA tests are available and the PER test shows the decoded frames.

Fixed issues :

  • Fixes the blank popup message displayed when the script detects an error,
  • Includes workaround to prevent some freeze observed on a serial port with MacOS.
  • Disables the navigation link when the 802.15.4 receiver test is in progress,
  • Updates ST logo and colors,
  • Disables the start button as soon as the channel list is inconsistent in 802.15.4 PER multi-channel test,

Restrictions :

  • In the OTA Updater panel, the Image base address bytes are inverted. To flash at address 0xAABBCC, user must set 0xCCBBAA. The default value 0x7000 is working because it is equivalent to 0x007000 and inversion has no effect.
This topic has been closed for replies.
stephane.legargeant
ST Employee
Nov 24, 2020 12:53 PM UTC

This thread has been closed to avoid multiple conversations happening on the same thread. Please create a new thread if you wish to ask questions or discuss this update.

1 reply

stephane.legargeant
stephane.legargeantAuthorBest answer
ST Employee
Nov 24, 2020 12:53 PM UTC

This thread has been closed to avoid multiple conversations happening on the same thread. Please create a new thread if you wish to ask questions or discuss this update.