Skip to main content
connoisseur_de_mimi
Associate III
December 10, 2025
Question

STM32CubeMonitor-RF: Scripting BLE Tests

I want to use STM32CubeMonitor-RF's scripting feature to automate BLE tests, but I'm having troubles right from the start: 

Send(ACI_GAP_CREATE_CONNECTION;0x01D0;0x01D0;0x00;<client address>;0x00;0x0040;0x0040;0x0000;0x015E;0x0015;0x0015)
Wait(500)
Send(ACI_GATT_DISC_ALL_PRIMARY_SERVICES;<connection handle>)

ACI_GATT_DISC_ALL_PRIMARY_SERVICES needs a connection handle, which is only known at runtime, it would need to be extracted from a response to the ACI_GAP_CREATE_CONNECTION command. is this possible, or is it possible to set the handle to a constant value?

    3 replies

    Richard.Chvr
    ST Technical Moderator
    December 10, 2025

    Hello @connoisseur_de_mimi, no possibility to extract handle from response nor to set in a constant value. In most cases, handle does not change in between script executions loop, need to get it value at first execution and use this value in script.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
    connoisseur_de_mimi
    Associate III
    January 28, 2026

    Unfortunately this seems not to work. Consider this simple script:

    # Script recording starts on 11/12/2025 19:25:34
    Send(ACI_GAP_CREATE_CONNECTION;0x0004;0x0004;0x00;0x000000000000;0x00;0x0006;0x0006;0x0000;0x000A;0x0000;0x0000)
    Wait(500)
    Send(ACI_GATT_DISC_ALL_PRIMARY_SERVICES;0x080A)
    Wait(1000)
    Send(ACI_GAP_TERMINATE;0x080A;0x13)
    # Script recording ends on 11/12/2025 19:26:40

    The first run is successful: 

    SCRIPT REPORT
    
    Script name : myScript2.txt
    Test date : 28/01/2026 10:35:20
    
    Verdict : SUCCESS No error detected
    
    Command | Sent | ACI status | ACI raw result
    ACI_GAP_CREATE_CONNECTION | OK | 0x00 | [0x04,0x3E,0x1F,0x0A,0x00,0x0A,0x08,0x00,0x00,0x4E,0x81,0x26,0xE1,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x06,0x00,0x00,0x00,0x0A,0x00,0x00]
    ACI_GATT_DISC_ALL_PRIMARY_SERVICES | OK | 0x00 | [0x04,0x0F,0x04,0x00,0x01,0x12,0xFD]
    ACI_GAP_TERMINATE | OK | 0x00 | [0x04,0x0F,0x04,0x00,0x01,0x93,0xFC]
    
    END of report

    runs after that fail: 

    SCRIPT REPORT
    
    Script name : myScript2.txt
    Test date : 28/01/2026 10:35:25
    
    Verdict : FAILED Some error have been detected
    
    Command | Sent | ACI status | ACI raw result
    ACI_GAP_CREATE_CONNECTION | OK | 0x00 | [0x04,0x3E,0x1F,0x0A,0x00,0x0B,0x08,0x00,0x00,0x4E,0x81,0x26,0xE1,0x80,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x00,0x06,0x00,0x00,0x00,0x0A,0x00,0x00]
    ACI_GATT_DISC_ALL_PRIMARY_SERVICES | OK | 0x0C | [0x04,0x0F,0x04,0x0C,0x01,0x12,0xFD]
    ACI_GAP_TERMINATE | OK | 0x00 | [0x04,0x0F,0x04,0x00,0x01,0x93,0xFC]
    
    END of report

    unless the connection handle is manually incremented. 

    CubeMon-RF log file attached. 

    Richard.Chvr
    ST Technical Moderator
    January 28, 2026

    You can use Loop to increment the connection handle

     

    Loop (CHandle, 0x080a, 0x0EFF)
    
    Send(ACI_GAP_CREATE_CONNECTION;0x0004;0x0004;0x00;0x000000000000;0x00;0x0006;0x0006;0x0000;0x000A;0x0000;0x0000)
    Wait(500)
    Send(ACI_GATT_DISC_ALL_PRIMARY_SERVICES;[CHandle])
    Wait(1000)
    Send(ACI_GAP_TERMINATE;[CHandle];0x13)
    
    Pause("Validate for next loop")
    
    EndLoop

     

    I don't know the the exact condition to avoid ConnectionHandle increment on remote device.

    To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.